Hi Alicia,
I think W&S mode is the best choice for customer.
Could you please help to provide the EVM power consumption test on the following conditions by today? Customer needs the data to have a comparison with competitor, so that they can keep…
Part Number: TMAG3001 Tool/software: Hello TI,
in a new project, I have to replace a level sensor design that uses hall switches. The goal is to get a continuous fluid level value..
Depending on the length of the device, I will need up to 40 sensors…
Part Number: TMAG3001 Tool/software: Dear,
We plan to use TMAG3001 component on one off our new design.
Electronic data are clear for us.
We have question about mechanical position of hall element in the case.
Datasheet indicate 0.25mm from top but 0…
Part Number: TMAG3001 Tool/software: I understand I can power this sensor from the same switched regulated supply which powers the bulk of my system including the microcontroller, memory etc But is the performance expected to be better if it is powered…
Part Number: TMAG3001 Hello, page 62 of the datasheet lists the available interrupt modes, which can be set by the "INT_MODE[2:0]" bits of register "INT_Config_1." I am unclear on the difference between the "Interrupt through INT" mode (1h) and the "Interrupt…
Hi Mustafa,
I am going to close this thread for now due to inactivity. Please let feel free to reopen this thread or ask a related question (if this thread has been locked) if you have any additional questions. If your question has been resolved, please…
Part Number: TMAG3001 Hi,
I'm looking for a sensor for a device that records trajectories drawn freehand.
Are TI products releasing sensors that output the amount of movement in x and y coordinates, such as those used in mouse computers?
Thanks, …
Part Number: TMAG3001 Other Parts Discussed in Thread: TMAG5273 , TMAG5253 We have an application that incorporates a joystick mechanism, and we currently use a Melexis 90333 Hall Effect sensor that is mounted with the Hall plate on the intersection of…
Part Number: TMAG3001EVM Other Parts Discussed in Thread: TMAG3001 , MSP-EXP432E401Y , MSP432E401Y , Tool/software: 1) How do I get the drivers and download programs to test the TMAG3001 with MSP-EXP432E401Y development board?
2) Is there C source code I…
Hi Alicia,
We have now managed to find a windows PC and tried the TMAG3001 sensor. I was able to run that tmag3001evm-bsl bat file, with no error, the GUI (both the browser and the installed GUI) can recognize the MSP432, but not the TMAG3001. It keeps…