Part Number: TMAG5124-Q1 We are testing the hall sensor TMAG5124-Q1 for position detection of the linear movement in a spindle with magnet. At commissioning some prototypes we noticed that, in some cases, the hall sensors do not start up correctly. During…
Part Number: TMAG5124-Q1 Hi
As shown in the image, if the TMAG5124F1CQDBZR is to be directly soldered to the pins, what precautions or suggestions are there?
Part Number: TMAG5124-Q1 Tool/software: I wanted to use TIMSS to simulate this part but the program does not work in Edge or Chrome on different computers.
Selection bars for simulation type etc do not display.
Part Number: TMAG5124-Q1 Other Parts Discussed in Thread: DRV5023-Q1 , TMAG5123-Q1 Hi,
TMAG5124G is the current output sensor. Is there any voltage output hall sensor with same Bop & Brp available?
Thanks
Part Number: TMAG5124-Q1 Hi,
The graphs given in the catalog for TMAG5124G are for supply voltage of 3V-12V. Vcc requirement in my application is 28V +/- 10%. Could you please provide the graphs for the same. Thanks
Part Number: TMAG5124 Other Parts Discussed in Thread: , DRV5055 Hello, I'm looking for a product that starts at 0mm and switches when it reaches 1mm. I have identified the TMAG5124 product. I checked the datasheet example to have a minimum magnet distance…
Part Number: TMAG5124
Hi,
Customer would like to design with a Low-Side Sensing Diagram.
Is it acceptable if the resistance value of Rsense is higher (ex. 150kOhm) or lower (ex. 100Ohm) than 220Ohm stated in the data sheet? If unacceptable, what…