Hi Chad,
I hope the suggestions and app note in my previous post were helpful. Please let me know if I can continue to provide support here. For now, I will be closing this thread.
Best regards,
Jesse
Part Number: TMAG5170
Hello,
As we are working in the aeronatic field, we have some constraints related to effects of ionizing particles (SEU).
Considering the fact that the TMAG5170 embeds a digital core and not knowing what it contains exactly, we…
Part Number: TMAG5170 Other Parts Discussed in Thread: DRV5056 , , DRV5055 I'm using the TMAG5170A1 to sense the linear displacement of a magnet. The system voltage varies from 2.5 V to 3.8 V. The Y and Z axes are used in the calculation.
I may have…
Other Parts Discussed in Thread: TMAG5170 Now we have question for continuous mode. I see registers and if understand well 010b = 2h, in active measurement mode is always low power mode time delay. So this mode is for our purpose (motor commutation ) not…
Part Number: TMAG5170-Q1 Hi team,
Considering using ALERT pin tied to GND, could you answer lower questions?
(1) Which resistor will be affected compared with ALERT pin is tied to VCC through pull up resistor? Is the only resistor affected by ALERT pin…
Part Number: TMAG5170-Q1 Hi team,
If we do not use ALERT fucntion and pin, how we handle ALERT pin connection? (Tied to GND, floating, tied to VCC through resistor?)
Regards, Ochi
Part Number: TMAG5170 Dears,
I'm in progress of writing SPI driver for TMAG5170 sensor. So far I created part with the automatic triggers (continuous conversion & duty-cycled modes) and they are working fine. Now I want to move to manual trigger modes…
Part Number: TMAG5170-Q1 Hi team,
How much measurement result error of X_CH_RESULT, Y_CH_RESULT, and Z_CH_RESULT without considering hall element location deviation do we expect?
For example TMAG5170-Q1 exposed actual flux densitiy Bx is 120.11223 mT, th…
Part Number: TMAG5170 Hi,
I have question about behaviour of RDY bit in CONV_STATUS.
When exactly this bit is setted to 1?
In our application we are triggering conversion via cmd bits and after about 1.8 - 1.9 ms we are reading conv_status and measurement…
Part Number: TMAG5170-Q1 Hi team,
"GAIN_VALUE" says that "The gain value is anywhere between 0 and 2 . Gain is calculated as 'user entered value/1024" shiown in " Table 7-23. MAG_GAIN_CONFIG Register Field Descriptions." However…