Part Number: TMAG5170-Q1 Other Parts Discussed in Thread: TMAG5170 Hi, TI team
Does the 3D hall sensor TMAG5170-Q1 support the following application?
is there any difference compare to the on shaft application, like the angle accuracy?
below is the on…
Part Number: TMAG5170-Q1 Other Parts Discussed in Thread: TMAG5170 Hi Team,
We are using the TMAG5170-Q1, We are able to get the sensor data when the sensor is operating in DEVICE_CONFIG_OPERATING_MODE_ActiveMeasureMode.
my application demands data only…
Part Number: TMAG5170-Q1 Other Parts Discussed in Thread: TMAG5173-Q1 , TMAG6180-Q1 Hello TI expert,
I saw TI also have Hall sensor with automotive grade , does Ti has Hall sensor angle detection less than ±0.5° in full temperature range?
…
Part Number: TMAG5170-Q1 Dear,
One customer need to confirm about the TMAG5170-Q1, since each product is different according to the position error and magnet filling error will cause the magnetic sensitivity of the HAL , how should we define the zero position…
Part Number: TMAG5170-Q1 Hello team,
What is the mechanical tolerance for the Hall sensor position inside of TMAG5170-Q1? X, Y and Z?
Best regards, Antoine
Part Number: TMAG5170-Q1 Other Parts Discussed in Thread: TMAG5170 Hi,
I have problem with the SET_COUNT value on the MISO line when starting a conversion via "CS going high" command.
According to the datahseet TMAG5170 shall start the conversion…
Part Number: TMAG5170-Q1 Other Parts Discussed in Thread: TMAG5170
Hello Expert
We plan to useTMAG517 to detect a magnet (with only NS polarity) rotating 150 °, which is fixed on the rotating axis
Could you help confirm if all of them can be implemented…
Part Number: TMAG5173-Q1 Other Parts Discussed in Thread: TMAG5170 , , TMAG5170-Q1 Hi,
435 / 5,000
I am preparing to use a 3D Hall effect sensor = comparing TMAG5173 and TMAG5170 there are a few differences: 5170: SPI, 8…
Part Number: TMAG5170-Q1 Hi team,
Considering using ALERT pin tied to GND, could you answer lower questions?
(1) Which resistor will be affected compared with ALERT pin is tied to VCC through pull up resistor? Is the only resistor affected by ALERT pin…
Part Number: TMAG5170-Q1 Hi team,
If we do not use ALERT fucntion and pin, how we handle ALERT pin connection? (Tied to GND, floating, tied to VCC through resistor?)
Regards, Ochi