Part Number: TMAG5273 Dear TI Engineer,
We are planning to use TMAG5273 in battery powered applications, hoping to achieve maximum power savings while meeting functional requirements. Therefore, we have the following questions that we need your help…
Part Number: TMAG5273 Hello,
I'm using the TMAG5273 IC, but I have one issue. If I change the I2C address of the TMAG5273, then after a power cycle, will the address return to the default address or remain the same?
If it changes back to the default…
Part Number: TMAG5273 Hello,
I use the TMAG5273 magnet sensor in an embedded project. I have added the chip in the dts with:
&i2c2 {
clock-frequency = <400000>;
pinctrl-names = "default", "gpio";
pinctrl-0 = <&pinctrl_i2c2>;
pinctrl-1 = <&pinctrl_i2c2_gpio…
Part Number: TMAG5273 Hi,
I am designing an industrial relay board and need to sense a magnetic field of ±200 mT. I found the TMAG5273 sensing IC, but I think it is more suitable for 3D joysticks and similar applications. Can I use the TMAG5273 for…
Part Number: TMAG5273 Goodmorning,
I'd like to ask a detail about the inside 3D Hall-sensor location refered to package dimension quote.
In the datasheet it is illustrated as a shifted location of 0.68x1.85mm from the top-left corner in top view with…
Part Number: TMAG5273 Continuing from this earlier discussion :
The behaviour described there can be generalised this like this: if you have (at least) two devices on a single I2C bus, and are using both tx and rx commands, alternating between the two…
Part Number: TMAG5273 Other Parts Discussed in Thread: TMAG5173-Q1 , TMAG3001 , TMAG5134 , TMAG5231 , TMAG5133 , DRV5032 , TMAG5230 Hello,
We are evaluating the TMAG5273 for a battery-powered smart lock application, where ultra-low standby current is…
Part Number: TMAG5273 Hi team,
We are currently using your TMAG5273A1QDBVR 3-axis Hall effect sensor in our projects.
I would like to inquire if you have any recommended methods or best practices for testing the X/Y/Z 3-axis open/short status (or…
Part Number: TMAG5273 I want to know the behaviourof the TMAG5273 when it'snot powered but still connected to the I2C bus with communicaition going on.
Part Number: TMAG5273 Tool/software: Hi, our current design includes a TMAG5273 sensor, we are powering it via a battery and using it for tamper protection. My question is that if the power to TMAG5273 is lost and an interrupt is generated before the…