Part Number: TMAG5273 Hi Team,
Could you pls comments on the maximum rate at which I2C reports angle information when the TMAG5273 is used in motor angle sensing applications? Thanks!
Regards, Hailiang
Part Number: TMAG5273
There is a strange issue, within the trigger threshold range, entering ws mode will immediately wake up. For example, if the current magnetic field intensity is 1mT and I set the threshold to be less than 1.25mT, an interrupt will…
Part Number: TMAG5273
We are designing a PCB and would like to place the TMAG5273 sensor such that the hall elements are at a specific location on the board. From the datasheet, the hall element location is referenced to the edge of the package rather…
Part Number: TMAG5273 Other Parts Discussed in Thread: TMAG5X73-CODE-EXAMPLE , Hi all,
We have selected this part for the one of our applications.
We are going to use TI (cc2340) controller as master.
Please provide us sample I2C Software driver for this…
Part Number: TMAG5273 My device contains a TMAG5273 array, which contains 16 TMAG5273 devices. How can I assign IDs to them and distinguish the correspondence between data and device ID.
For the IIC communication in the datasheet:
Table 7-20. I2C_ADDRESS…
Part Number: TMAG5273 I am writing to device config register following address to put it in continues measurement mode.
self ._write( 0x 01 , '\x02' )
I can write without error but reading it back always gives 0x78. So I can not verify device config…
Part Number: TMAG5273 Other Parts Discussed in Thread: TMAG5173-Q1 I have two questions about the TMAG5273A1 --
What is the output resolution of the CORDIC? I see it specified in the datasheet for the TMAG5173-Q1 but not this part.
How do I interpret MAGNITUDE_RESULT…
Part Number: TMAG5273 Hello,
I am trying to get some clarification on the magnetic axis modes described in SENSOR_CONFIG_1 register table. I understand the individual axes being on or off, but what is meant by modes XYX, YXY, YZY, and XZX (modes 8h -…