Part Number: TMCS1123 Other Parts Discussed in Thread: TMCS1107EVM Tool/software: What is the best hall-effect current sensor for measuring DC current, ranging from 1A to 85A with Vs=3.3V. Thank you
Part Number: TMCS1107 Tool/software: Hi TI Support,
I need assistance with a TMCS1107 100mV/A current sensor. I have connected it with 3.5Vdc on Vs and GND, but I am not able to measure anything on Vout. My test load is 7A between IN+ and IN-. I am…
Part Number: TMCS1107 I am trying to use the TMCS1107 in Pspice for TI and am coming across an .olb file error. I already redownloaded the TI libraries through the help tab. Any idea?
Part Number: TMCS1107 Other Parts Discussed in Thread: TMCS1126 Tool/software: Hello team,
What is the safety limiting value?
Side 1 and 2 mean two area separated by isolation barrier. Is this correct?
If yes, TMCS1107A1U should sense the current…
Part Number: TMCS1107 Other Parts Discussed in Thread: TMCS1101 Tool/software: Dear TI experts,
My customer wants to check IEC 62368-1 certification for the 2 devices below ;
TMCS1107A2B
TMCS1101A2B
Could you check the certification of these 2…
Part Number: TMCS1107
Hi, For TMCS1107A4B, the sensitivity is given as 400mV/A, when the IC is biased with 5V.
Sensitivity = delV_out/sensing_current_Range (as mentioned in the datasheet)
Which comes out to be around 400mV/A.
My question is, if…
Part Number: TMCS1107 Hi Team
do you think TMCS1107 is best solution to replace ACS37612?
Please see attached file is data sheet.
acs37612-datasheet.pdf
BRs
Brian
Part Number: TMCS1107-Q1 Other Parts Discussed in Thread: TMCS1107 Hello,
I am utilizing the TMCS1107A1BQDRQ1 IC for measuring current in both AC and DC loads. When testing DC load, I observed that the output voltage of the IC change depending on whether…