Part Number: TMCS1126 Hi
The TMCS1126 datasheet specifies a maximum capacitive load of 20nF for the VREF pin but lacks a minimum value.
My customer plans to place a 1nF capacitor on VREF for noise filtering. Is 1nF acceptable, or will it cause buffer…
Part Number: TMCS1126 Hi
In a TMCS1126 design, the overcurrent feature is unused, and the customer tied the OC pin directly to GND . Could you confirm the following?
Even if an internal overcurrent fault triggers, will shorting the OC pin to GND…
Part Number: TMCS1126 Dear Sir,
I am using the TMCS1126C4 current sensor with the following configuration:
VS = 3.3 V Overcurrent threshold voltage (VOC) = 0.075 V R1 = 43 kohm R2 = 1 kohm Calculated overcurrent set point = approximately 1.8 A
When…
Part Number: TMCS1126 Hi,
Can I get assistance with an issue where Vout gain toggles for short durations of approximately 20- 25 ms, non-periodically, using TMCS1126B6AQDVGRQ1? Vs and Vref has been checked at is stable during fault. The filter used…
Part Number: TMCS1126 Hello Sensing team,
My customer is looking into the TMCS1126A1A and TMCS1126A1B.
they want to understand the pinout connection, see figure below.
Is it possible to connect PIN 10 to Vs (+5V)?
Kind regards,
Wouter…
Part Number: TMCS1126 Dear Technical Support Team,
I am researching the TMCS1126.
The following are the specifications I am considering. Could you please let me know if there are any precautions to take when using this device, or if there are other…
Part Number: TMCS1126 Other Parts Discussed in Thread: UCC14141-Q1 Tool/software: TMCS1126 and UCC1414 have planned certifications per IEC 60747 and UL1577. Has the required testing for these certifications been completed and what date is certification…
Part Number: TMCS1126-Q1 Other Parts Discussed in Thread: TMCS1126 Hi E2E,
We are designing a compressor application of automotive. TMCS1126-Q1 is used for current detection and protection. We found that when the motor is working normally, there will…
Part Number: TMCS1126
We are using the TI TMCS1126A1B and are observing a random change of sensitivity doing operation. Is this a predicted failure mode caused by something obviously that we missed. We followed the application layout, but see a freshly…
Part Number: TMCS1126 Hi,
we want to use the TMCS1126 as well as some alternative part in similar SO16 package. Is there any application note or footprint recomondation for a combined layout?
Kind Reguards