Part Number: TMCS1126 Tool/software: Hi there,
This is Racheal from AA3 team in Shenzhen. My customer is now using TMCS1126 in PFC current detection. When the power ramping up, the output signal of TMCS1126 is toggling with amplitude of 60mV, shown…
Part Number: TMCS1126-Q1 Tool/software: HI~
TMCS1126A7AQDVGR-Q1 is being used, and the understanding Vref is shaken by noise, so the cap is designed by applying 1uF.
If I look at the application notes, Vref is 4.7nF and 20nF, what is the problem if…
Part Number: TMCS1126EVM Other Parts Discussed in Thread: TMCS1126 Tool/software: Team,
The TMCS1126 EVM User guide document doen't show the Grade A or Grade B information for TMCS1126 which is mounted on the EVM. Refer to the below capture for TMCS1126A…
Part Number: TMCS1126 Tool/software: Hello,
Need 3D body for the part number TMCS1126A1BQDVGR.
Please share the 3D model as soon as possible to proceed further.
Part Number: TMCS1126-Q1 Other Parts Discussed in Thread: TMCS1126 Tool/software: Hi~
Please tell me the current consumed from TMCS1126-Q1 VS pin(Power supply)
Part Number: TMCS1126 Tool/software: If I have a close-loop controller with a dc motor using Ripple Current for position/counts and would like to measure the counts external from this system do you have a recommendation?
Part Number: TMCS1126-Q1 Tool/software: HI~
Q1) I saw in the data sheet that Vref has 2.5V output from VCC 3.5V to 5V
Q1-1) Is this condition 3.3V to 5V or is it only satisfied at 3.3V and 5V?
Q2-1) Is there any data where Vref has been measured…
Part Number: TMCS1126-Q1 Other Parts Discussed in Thread: TMCS1126 , TMCS1123 Tool/software: Hi
I want to know TMCS1126-Q1 lifetime (available period)
I looked up the data sheet, but I couldn't find an answer
I want to check all the temperature…
Part Number: TMCS1126-Q1 Other Parts Discussed in Thread: TMCS1100-Q1 Tool/software: Hi Team,
What is the input voltage range allowable for the IN+ and IN- pins of TMCS1126-Q1? We haven't seen this in the datasheet.
I see that this parameter is available…
Part Number: TMCS1126 Tool/software: Hi team,
With OC pull up to VS, when test OC pin during power down, there is many glitch on OC pin. In below waveform, blue is VS. purple is OC pin. you can see significant glitches during power down. After zoom…