Part Number: TMCS1133 Hello TI Team,
I am reviewing the PM23603 reference design and have a question regarding the LLC converter transformer connections.
In the schematic, the TMCS1133 Hall-effect current sensor is connected through the nets PPL_P1…
Part Number: TMCS1133 In one of our projects the TMCS1133C1A current sensor is used to sense LLC converter input current.
The sensor measures a 100kHz rectified sinusoidal current of 50A-60A (peak value) but a strange behavior happens on sensor output…
Part Number: TMCS1133-Q1 Other Parts Discussed in Thread: TMCS1133 Tool/software: TMCS1133A1AQDVGR it's a sensor very interesting , good bandwith, time delay, current.
Have a sensor equivalent with higher current (higher 90A) capability ? Do you have…
Part Number: TMCS1133-Q1 Other Parts Discussed in Thread: TMCS1133 , TMCS1148 , , TMCS1143 Hi team,
We are using TMCS1133B1 in discharger project and its package temp is up to 110C and customer can not accept it.
TMCS1133's Rdson is 0.7m ohm. Do we…
Part Number: TMCS1133-Q1 Other Parts Discussed in Thread: TMCS1133 Hello?
I am writing to inform you that during our recent 2kV surge immunity test on our product, the unit sustained damage specifically affecting the TMSC1133 component. Following the…
Part Number: TMCS1133 Tool/software:
The sensitivity thermal drift shows +/-20ppm/degC, it means 20ppm/degC= (20/1e6)*190*100=+/-0.38%. But the fig 6-1 shows it is only -0.1% error. What's different?
Part Number: TMCS1133-Q1 Other Parts Discussed in Thread: TMCS1133 Hi team,
in context of accuracy calculations for the TMCS1133 sensor a few questions regarding the error contribution due to the external magnetic field came up at my customer. According…
Part Number: TMCS1133 In a DAB application we are seeing OC trips under higher load conditions. When we measure the current it is far below the trip level. We have a feeling that it might be related to the temperature but we are not entirely sure. The…
Part Number: TMCS1133 Hi TI Team,
Do TMCS1133 curves in datasheet figures 7-5 through 7-8 (Maximum Repetitive Pulsed Current vs. Pulse Duration) show the peak pulsed current (I_IN,P) or the RMS peak pulsed current (I_IN,RMS)?
Many Thanks in advance…
Part Number: TMCS1133 Hello, I would like to clarify the statement from the datasheet:
"This fast digital response can be configured on both bidirectional and unidirectional devices to assert based on a signal that is anywhere from half to over twice…