Hi,
Glad to see the data sheets recently updated. Still, there are some things which does not seem clear enough. In particular:
Each the part implements the Rx Pattern Verifier Control/Status register. The register has PV_LD[3:0] field which is defined…
Other Parts Discussed in Thread: TMDS181 , TMDS171 Hi,
Which performance of TMDS171 and TMDS181 is excellent if using TMDS171 and TMDS181 with data rates up to 3.4Gbps in the retimer mode ? In addition, could you please let us know that reason ?
Best…
Hi Moises-san,
Please allow me to ask you again. I would like to make clear about the requirement.
Our customer is only using 0.1uF cap at the OE pin in their schematic, however, OE pin voltage will rise above VIL=0.8V before 3.3V is stable. I believe…
Hello Moises-san,
I understood that the VIM spec voltage range is the required output level from the external controller devices. Thank you for the information.
Best Regards,
Kawai
Other Parts Discussed in Thread: TMDS171 Hi My customer is using TMDS171 EVM. www.tij.co.jp/.../sllu217.pdf He wants Eye Scan software. Could you send me this software? or Could you let me know download web?
Best regards Shimizu
Part Number: SN65DP149 Other Parts Discussed in Thread: TMDS181 , TMDS171 Hi,
I am writeing in regrds to the compatibility of SN65DP159RSBR and SN65DP149RSBR they are HDMI retimers and if i use the QFN-40 footprint i see them as equivalent. I want a…
Part Number: TMDS181 Other Parts Discussed in Thread: TMDS171 Hi,
The product is a redriver for HDMI1.4b with data rates up to 3.4 Gbps.
Is the product Compatible with HDMI1.4 (not HDMI1.4b)?
Regards
Einav