Part Number: TMDS64EVM Other Parts Discussed in Thread: SYSCONFIG Hello Ti,
I am using TMDS64EVM Board with Linux(Debian preemt_rt) and MCU+SDK 09.01.00v
I have implemented the ipc between the R5 and M4 core with CCS and Now i am trying to implement with…
Hello Raj,
Raj Kumar said: 1.Since it is a ipc example ,we have to build as a system project and i have made some changes with ccs so, how can i build it as a system project in ccs?
To build the IPC RPMSG echo example for R5F0-0 and M4F0-0 core, please…
Hi Shraddha,
shraddha naik said: One query i had is where is my u-boot images stored here?? Can you tell me how to check this?
The U-Boot images are stored in the eMMC Boot0 hardware partition while the Linux filesystem is stored in the eMMC UDA partition…
Hi Jonas,
So we tried to reproduce the issue by keeping a non TI device (EL9800) as first device and AM64x EVM as 2nd device and measured the SYNC pulse of AM64x with respect to EL9800 but we weren't able to see the jitter happening around 91ns. In our…
Ok, so you are not just looking for a DUT to configure as either cut-through or store and forward. I would still recommend trying this as a reference with Linux as the switch configuration with the default SDK SD card image is quite quick.
As you have…
Part Number: TMDS64EVM Hello, TI support team.
I have two questions about the interrupt controller in TMDS64EVM.
In my system, a peripheral timer (TIMERx, one of x=0-11) interrupts two CPUs in parallel with the following configuration:
TIMERx's…
Part Number: TMDS64EVM Hello TI support team.
Please tell me about CR5's DMTIMER interrupt. Set the interrupt priority of DMTIMER0 to 1. Is it possible to change the interrupt priority to 3 and back to 1 in the DMTIMER0 interrupt handler? I would like…
Hello Kiyomasa,
Kiyomasa Imaizumi said: I attach the latest data obtained with ospi_flash_diag.
It seems like the ospi_flash_diag somehow is not working correctly for IS25LX256 flash.
Kiyomasa Imaizumi said: does that mean that the json file in the SDK…
Part Number: TMDS64EVM Hi,
I was referring the TMDS64EVM schematic PROC101D(004) and found one MDC/MDIO FET switch.
Can anyone help me to understand the use case of this circuit in the design.
If I am using the PRG1 interface, PRG1_MDIO/MDC (Y6/AA6) only…
Part Number: TMDS64EVM Hello TI support team.
I'm using IPC RPMessage with CA53 and CR5.
CA53 is the master and CR5 is the slave. I think RPMessage_recvHandler is called in CR5 when sending from CA53. I would like to send a message to CA53 within the…