Yes. We have provided a software FAST library based solution that can support InstaSPIN with FAST on all of the C2000 devices with FPU. You may refer to the lab for the newer C2000 device in motor control SDK. The universal motor control lab is available…
the 3-ph inverter boards are the same / compatible with any of the controlCARDs.
There is older controlSUITE examples for TMDSCNCDF28835, TMDSCNCD28035
and older MotorWare examples for TMDSCNCD28069MISO, TMDSCNCD28054MISO, TMDSCNCD28027F
and newer…
We have provided a software FAST library based solution that can support InstaSPIN with FAST on all of the C2000 devices with FPU. You may refer to the lab for the newer C2000 device in motor control SDK. The universal motor control lab is available in…
What maximum current and voltage do you need for the motor drive? You can refer to the table below to select a replacement.
Universal Motor Control Lab with Sensorless -FOC (InstaSPIN-FAST/ eSMO ) or Sensored-FOC(Incremental Encoder) for BLDC…
You may take a look at the application note of the example project that has the detailed description of the questions you mentioned above. You can try to follow the guide to run the lelvel1 to level7 for understanding how to tune the example.
If you…
We have provided a softwareFAST library that can support InstaSPIN with FAST on all of the C2000 devices with FPU. You may refer to the lab for the newer C2000 device in motor control SDK. And refer to the lab user's guide to migrate this lab to the C2000…
Yes. You may refer to the Universal Motor Control Lab in the latest motor control SDK as below. The project may have a little different to the project you are using, but you can still refer to the program flow to implement it. Or you can use the Universal…
We have provided a softwareFAST library that can support InstaSPIN with FAST on all of the C2000 devices with FPU. You may refer to the lab for the newer C2000 device in motor control SDK. The universal motor control lab is available in the current MCSDK…
You may refer to the lab for the newer C2000 device in motor control SDK. The universal motor control lab is available in the current MCSDK, which can support a set of hardware kits and control algorithms for BLDC/PMSM drive. The kits include LAUNCHXL…
Yes, these 3 controlCards can support InstaSPIN labs in motorWare.
Or you may refer to the lab for the newer C2000 devices in motor control SDK. The universal motor control lab is available in the current MCSDK, which can support a set of hardware kits…