Hi,
Filipe Carneiro said: To connect the TMDSCNCD280025C controlCARD to the host computer via SCI, is it only necessary to set S1:A pos 2 to ON or is there something else I am missing
I think that is correct.
Are you still having this issue?
Thanks,
Ben…
Part Number: TMDSCNCD280025C Hello! I wanted to implement basic uart. This is the program that I've written. I'm stuck on how to display the values of different variables by using %d, %s etc. In the program below, I've printed a basic string.…
Part Number: TMDSCNCD280025C Other Parts Discussed in Thread: C2000WARE Hello, I am doing a project where I am planning to use the TMDSCNCD280025C for a battery management system.
I was wondering where I can find the schematics for this evaluation module…
Part Number: TMDSCNCD280025C The TMDSCNCD280025C datasheet mentions that there are 8 High Resolution PWM channels out of the 14 PWM channels. However I can't find any information on which of those 14 PWM channels are the High resolution channels. If anyone…
Part Number: TMDSCNCD280025C I am currently trying to connect to the control card mentioned above via a USB connection without a docking station. When attempting to use CCS to connect to my board I am given the error "2131 - Unable to access device register…
Part Number: TMDSCNCD280025C Hi,
<Phenomenon> In the past, the debugger and target were successfully connected, but a connection error occurred immediately after loading the program, and the target could not be connected after that. I did the following…
Part Number: TMDSCNCD280025C Other Parts Discussed in Thread: DRV8353RS-EVM Dear support team.
I have successfully run one of our motor using DRV8353RS-EVM + TMDSCNCD280025C.
This motor was properly identified using DMC level 4.
The result was something…
Part Number: TMDSCNCD280025C Other Parts Discussed in Thread: TMDSHSECDOCK , CODECOMPOSER I have the control card plugged into a TMDSHSECDOCK docking station and it's been working fine with the on-board XDS100v2 USB interface. However I want to verify that…
Part Number: TMS320F280025C Other Parts Discussed in Thread: TMDSCNCD280025C
Hi Team,
TMS320F28002x supports InstaSPIN-FOC.
My customer wants to use InstaSPIN gui with TMDSCNCD280025C and their motor to confirm motor control parameters
How to…
Part Number: TMDSCNCD280025C Other Parts Discussed in Thread: C2000WARE
I have been working on SPI Boot mode for C20025C. I have an external Flash connected to my DSP control card(TMDSCNCD280025C) over SPI.
So, the procedure I am following is this.
…