You can reference the F28027 controlcard and launchpad schematics in C2000Ware to assist with debug.
C:\ti\c2000\C2000Ware_1_00_01_00\boards\LaunchPads\LAUNCHXL_F28027
C:\ti\c2000\C2000Ware_1_00_01_00\boards\controlCARDs\TMDSCNCD28027
Best regards
…
Victor,
Porting application code from one device to another will be more difficult than modifying another example that is already built for your target platform.
Would you be able to use a Power Conversion example from this list that is built for F28027x…
certainly lower the bus voltage.
TMDSCNCD28027F is InstaSPIN enabled, the standard TMDSCNCD28027 is not
However, if you are going to use F2802x I suggest it is cheaper and better to just buy
LAUNCHXL-F28027F
and a boosterpack
BOOSTXL-DRV8301 (24V/10A…
Hi Roy,
What is the name of your development kit? Check it out from here: http://www.ti.com/product/TMS320F280270#toolssoftware
Does it look like this: http://www.ti.com/tool/tmdscncd28027
or is it a TMS320F28027 based C2000 Launchpad?
Regards,
Gauta…
it looks to me like a SW driver issue for the emulator. But if a pin is missing on the header of the DRV8301 that certainly could also be an issue.
I will also note that if using the TMDSCNCD28027 (or 27F) with the DRV8301 EVM you need to fix the enable…
Juha,
A constant 1V2 DC s not a voltage signal that the controlCARD should ever produce. I think something may be wrong with your card.
Why don't you try running a basic example program found within controlSUITE and seeing if you can flash the card properly…
I have the following two kits and the documentation for these can be found in controlSUITE: Controlstick: http://focus.ti.com/docs/toolsw/folders/print/tmds28027usb.html ControlCARD: http://focus.ti.com/docs/toolsw/folders/print/tmdscncd28027.html I was…
Kishor,
F2802x Workshop presentation and lab exercises should help you get started.
http://processors.wiki.ti.com/index.php/C2000_Archived_Workshops#C2000_Piccolo_One_Day_Workshop_-_Revision_2.1_December_2010_.28controlSTICK_F28027.3B_CCSv4.2.29
F28027…