InstaSPIN-FOC and InstaSPIN-MOTION can be run on the DRV8312 or DRV8301 EVM by purchasing
TMDSCNCD28069MISO or TMDSCNCD28027F
and using MotorWare
there is a "pre-compiled" GUI for use with 69M card, and a UNIVERSALGUI (whiich means you first compile…
By V/F do you mean "open loop" or "variable frequencey" (where things like FOC would be used).
In controlSUITE the primary series used for motor control development was F2803x. We then ported a few things to F2833x or co-built projects as F2806x.T …
1) there is no 62F controlCARD. 62F (and all the other F and M devices) are a subset of 69M. For all InstaSPIN-FOC & -MOTION controlCARD development you have two choices TMDSCNCD28069MISO or TMDSCNCD28027F. If you want to design your own board you can…
shailesh,
There is quite a lot of information, so I can understand being confused about www.ti.com/instaspin
Regarding the software architectures, this link should be helpful.
My advice is to learn InstaSPIN-FOC & InstaSPIN-MOTION in the following…
Keith,
Yeah, what you are seeing is the fact that we released InstaSPIN (and all the docs) for the first three kits over two years ago"
DRV8312-69M-KIT, DRV8301-69M-KIT, and TMDSHVMTRINSPIN all working with TMDSCNCD28069MISO controlCARD.
since…
Tim,
Do you mind staying a new thread since yours is a separate topic. I assume you are using the standard smo SW for your multi axis kit? Please include that info.
Roman,
The drv8302 is a nice device and a nice EVM. Do understand that there is…
There are a couple ways you can go.
InstaSPIN-BLDC
Likely Kit: DRV8301-HC-C2-KIT, configured for up to 60V/60A Piccolo device: default is CNCD28035 (included). CCS project can be rebuilt for CNCD28069
InstaSPIN-FOC
Likely Kit: DRV8301-69M-KIT…
TMDSHVMTRINSPIN 50-350V DC Bus (you provide bus or 110-230Vac input which is doubled to provide bus) 10A max controlCARDS: TMDSCNCD28069MISO (InstaSPIN-FOC & -MOTION) and TMDSCNCD28027F (InstaSPIN-FOC)
DRV8301-69M-KIT 15-60V DC Bus (you provide bus…
Omar,
To add some further clarity for posterity.
There are two paths for motor control development within the Piccolo line of MCUs.
1. controlSUITE: supports legacy Macro style Motor Library and InstaSPIN-BLDC
Projects are self contained to…
David,
Let's start over.
We have three main low voltage 3-ph inverter platforms that support different power levels
DRV8312 EVM: 50V/3.5A continuous
DRV8301 EVM: 60V/40A or 60V/60A (depending on if you use current sense that amplfies through…