Hi, Ken.
I think we've crossed our streams....we have a bunch of different solutions running on these boards and it can get pretty confusing.
DRV8312-C2-KIT
is supported through controlSUITE and has project that run on TMDSCNCD28035ISO (and dual…
Other Parts Discussed in Thread: MOTORWARE Trying to figure out how to setup the hardware/board for SCI/UAR design on the the development kit.
Here is the kit and control board I'm using:
1. development kit : http://www.ti.com/tool/TMDSHVMTRPFCKIT…
Hi Chris,
I'm trying to use SCI/UART communication to talk to PC. Could you please let me know how should I set it up?
I use the following board:
1. development kit : http://www.ti.com/tool/TMDSHVMTRPFCKIT?keyMatch=TMDSHVMTRPFCKIT&tisearch=Search…
Sean,
I was just making some other changes to that doc for the next MotorWare update (June to version _13).
Thanks for catching that. I checked the others and they are correct.
Attached is the new version of the doc that lives at
docs\boards\drive…
Part Number: LAUNCHXL-F28069M Other Parts Discussed in Thread: CCSTUDIO I am trying to spin a motor with a TI Booster Pack DRV8305EVM. Is there a version of this /cfs-file/__key/communityserver-discussions-components-files/171/qsg_5F00_gui_5F00_universal…
Hi Mojo,
first, note that for the InstaSPIN software with DRV8301 EVM we are using the external op-amps from the current sense, so you should look at the spec for the TLV devices.
second, the board was originally designed to sense about 82A peak …
Steve,
Please use the MotorWare InstaSPIN documentation and not the TI DMC Libraries. They follow the same philosophy of per unit, but the differences may confuse you.
The maximum range of input to the ADC pins is set by the hardware circuitry. The…
your Ls values are incorrect. The smallest real value would be a few uH
this would be for very high speed motors.
if you have one of these types of motor use proj_lab02c to identify (even just use your DRV8312 kit to make sure you get the right values…
attached QSG was accidently left out of MotorWare release, it belongs here
C:\ti\motorware\motorware_1_01_00_13\docs\guis\universal
there is also the QSGs for the "frozen" GUIs
C:\ti\motorware\motorware_1_01_00_13\docs\guis\hvkits_8312s_8301s
…