Part Number: TMDSCNCD28069MISO Other Parts Discussed in Thread: BOOSTXL-DRV8301 , DRV8301-HC-C2-KIT Hi Team,
According to 2.1 Overview of user guide below, TMDSCNCD28069MISO can be paired with BOOSTXL-DRV8301.
But after checking the picture of both I can…
Part Number: TMDSCNCD28069MISO I did transfer the Schematic files of the TMDSCNCD28069MISO to Altium schematic files via the Import Wizard. But it could not understand the .pcb file there. Opened the .pcb file with notepad and at some point we read C…
Part Number: TMDSCNCD28069MISO Hi,
is it posible to customize the Interface of the Universal GUI? Or do i need to creat my own GUI and use your APIs?
Thanks in advance
Part Number: TMDSCNCD28069MISO Other Parts Discussed in Thread: TMDSHVMTRINSPIN Hello,
While testing on TMDSHVMTRINSPIN development kit using TMDSCNCD28069MISO the Isolated JTAG was damaged.
Before connecting to the Mains, the development kit was connected…
Part Number: TMDSCNCD28054MISO Other Parts Discussed in Thread: TMDSCNCD28069MISO , , C2000WARE Prepare an EMB wheel end braking project. Can you help provide the schematic diagram of the development board of tmdscncd28054miso and tmdscncd28069miso,many…
Part Number: TMDSHVMTRINSPIN Other Parts Discussed in Thread: MOTORWARE , TMDSCNCD28069MISO , , TMDSCNCD28069ISO , CONTROLSUITE Hi, I'm using TMDSHVMTRINSPIN evaluation board and used TMDSCNCD28069MISO control card(that is broken during experiment) with…
I believe there is some divide by zero etc happening, i'll suggest re-looking at how you have instanced the SFRA in the application for the speed controller and make sure that you run only one instance.
So ensure SFRA speed is the only SFRA inject…
Suresh leley said: I was able to use both the Jtag and RS232 Port on the Mini USB when I plugged it in the low voltage drv8312 invertor.
If you can use them on DRV8312-kit, you can use them on the High Voltage kit also, you just need to insert jumper …
Part Number: TMDSCNCD28069MISO Other Parts Discussed in Thread: CONTROLSUITE
Hi there,
I am running the demo project PM_Sensorless for DRV830x-HC-C2-KIT_v105 in controlSUITE. I am testing the motor's encoder and it is connected to the MCU's eQEP module…
Part Number: TMDSCNCD28069MISO Other Parts Discussed in Thread: TMDSHVMTRINSPIN , TMDSCNCD280049C , TMDSADAP180TO100 , TMS320F280049C Hi Team,
We have a customer looking for a BLDC motor driver for a 36 pole three phase BLDC washing machine motor having…