Part Number: TMDSCNCD28335 Other Parts Discussed in Thread: CONTROLSUITE , C2000WARE , CCSTUDIO , SYSCONFIG , UNIFLASH Hello,
We are encoutering a problem using some examples on 28335. To be exact I work on a control card release 2.2, TMDSCNCD28335…
Part Number: TMDSCNCD28335 I am using TMDSCNCD28335 board. On CCS v6 I made test connection but the the test failed "The JTAG DR Integrity scan-test has failed" and LD1 turned off on the board but LD1 on the docking board is lightning.
I tried to change…
Part Number: TMDSCNCD28335 Other Parts Discussed in Thread: SN75HVD10 I am using SPI pins of F28335 DSP to read SSI output of a position encoder (Baumer:GA240.030R005000). For this purpose, I am using transceiver IC (75hvd10) to interface the differential…
Part Number: TMDSCNCD28335 I Try to run the DSP oscilloscope in PSIM with f28335 the PSIM example called " Monitoring 3-phase Sine Waveform through SCI (Serial Communication Interface)" .So, I turn SW1 off and short J9 in F28335 then generate the code…
Part Number: TMDSCNCD28335 I am using MAX488 IC to interface with SPI part of the DSP board F28335 with absolute encoder GA240.030R005000 to sense the position of Switched reluctance motor. An issue has shown as there was not any signal came out from…
Part Number: TMDSCNCD28335 Other Parts Discussed in Thread: C2000WARE Tool/software: I developed a firmware for SCI communication on a TI TMDSCNCD28335 prototype board. If I used the RAM linker file and debug with CCS, it worked fine. If I used the flash…
Part Number: TMDSCNCD28335 Other Parts Discussed in Thread: UCC21520 Tool/software: The TMDSCNCD28335 was used as a microinverter controller. The power supply of the board is independent of the main circuit.
The system works normally if the input voltage…
Part Number: TMDSCNCD28335 Other Parts Discussed in Thread: TMS320F28335 , TMDSDOCK28335 Tool/software: Hello,
I have a TMDSDOCK28335 (TMS320F28335 Experimenter Kit) and I've been experiencing some problems when I use it with Simulink in external…
Part Number: TMDSCNCD28335 Other Parts Discussed in Thread: TMDSDOCK28335 , Hello,
Is there a schematic available for the TMDSCNCD28335 daughter card? It appears only the certificate of conformity is available under technical documentation. I checked…
Part Number: TMDSCNCD28335 Greetings,
I am a beginner in microcontrollers programming. I got the TMDSCNCD28335 from a colleague. I am wondering how to completely erase any previously stored programs in the mentioned microcontroller memory.
Thanks…