Part Number: TMDSCNCD28P65X
Dear TI Team,
A customer has reported an issue with TMDSCNCD28P65X . The part is displaying an error and is not functioning properly.
Issue Details:
Number of defective units: 1
Is the error occurring immediately…
Part Number: TMDSCNCD28P65X Hi
Picking up from https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1638920/tms320c28346-pin-assignment-for-c28-dual-core-chip thread,
Here are two linker command…
Part Number: TMDSCNCD28P65X Tool/software: Hi,
On the TMDSCNCD28P65X board, both the F28P650 device and the EtherCAT PHY circuitry share a common 25MHz clock source.
I’d like to understand the rationale behind this design decision. Is it because…
Part Number: TMDSCNCD28P65X Other Parts Discussed in Thread: C2000WARE , SYSCONFIG Hi,
I am trying to segregate available RAM between CPU1 and CPU2 for 28p65 DSP. My starting point is the empty project provided with C2000Ware 6.x for this chip under…
Part Number: TMDSCNCD28P65X Other Parts Discussed in Thread: AM263P4 Good morning,
i want to drive an EtherCAT bus system with the F28P65 EvaluationCard. I just noticed, that i require a EtherCAT master. Is the F28P65 suited for the task? As I understood…
Part Number: TMS320F28P650DK Other Parts Discussed in Thread: TMDSCNCD28P65X , , TMDSHSECDOCK Dear Team,
We are planning to procure the TMDSCNCD28P65X controlCARD evaluation module for the MCU TMS320F28P650DK along with the docking station TMDSHSECDOCK…
Part Number: TMDSCNCD28P65X Other Parts Discussed in Thread: C2000WARE , UNIFLASH Tool/software: Hi TI team,
I'm studying the TMDSCNCD28P65X control card and trying to program some example code from C2000Ware_5_04_00_00 using CCS version is 12.8.1…
Part Number: TMDSCNCD28P65X Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hello there,
Got the SPI Module running at desired SPYCLK rate etc.
Trying to maximize the speed of SPYCLK up to 50 MHz of advertised limitation. Seems to be able…
Part Number: TMDSCNCD28P65X Tool/software: Hi,
I am having trouble figuring out the limits parameters in DCL_runPI_L1. Does it have both the integrator limit (Imax, Imin) and control limit(Umax,Umin) in the .asm? I cannot tell explicitly.
I need the…
Part Number: TMDSCNCD28P65X Other Parts Discussed in Thread: TIDM-DC-DC-BUCK Tool/software: Hi,
Do you have any examples on how I would be able to implement soft start on a buck converter in code? The goal is to control the increase of the output…