Part Number: TMDSCNCD28P65X Other Parts Discussed in Thread: TMDSCNCD28388D Tool/software: Hi,
When reviewing the circuit design of the TMDSCNCD28P65X, I noticed that both 20MHz and 25MHz clock sources are included. However, in practice, only the 25MHz…
Part Number: TMDSCNCD28P65X Tool/software: Hello,
I tried to follow the usb_ex1_dev_serial example. It worked perfectly fine however when I tried to implement in in my project the ControlHandler is never called. The txhandler and the rxhandler works…
Part Number: TMDSCNCD28P65X Tool/software: Recently, I bought two TMDSCNCD28P65X , one of them is able to connect to xds 110 and go to debug mode when I power it from J1 USB, but the other one is not. So I have two questions:
1. I wonder if I still…
Part Number: TMDSCNCD28P65X Tool/software: I am currently looking for a DSP solution for an automotive application with 20 PWM signals. I reviewed the C2000 MCUs like the TMDSCNCD28P65X and the TMDSSCNCD280039C, and saw that they only feature 16 ePWM…
Part Number: TMDSCNCD28P65X Other Parts Discussed in Thread: LAUNCHXL-F28P65X , C2000WARE Tool/software: We have successfully built the f28p65x_cpu1_echoback_solution example with the Slave Stack Code and can run it in the Code Composer Studio debugger…
Part Number: TMS320F28P650DK Other Parts Discussed in Thread: TMDSCNCD28P65X Tool/software: Hello everyone,
I'm currently working with the TMDSCNCD28P65X and I'm looking for sample code to facilitate UART/SPI communication with the BQ79600EVM-030 and…
Part Number: TMDSCNCD28P65X Tool/software: Good morning!
I try to log data received from an SCI bus on an SD card. The board has an included SD card slot on the SPI C. As I want a better reachable slot, I want to use an external SD card slot on another…
Part Number: TMDSCNCD28P65X Hi, customer has one of the first CC version E1. He can run the TI examples in RAM and also he can flash it with the debugger. But then it doesn't execute by its own. Boot pins are set to flash. He used latest CCS.
Regards…
Part Number: TMDSCNCD28P65X Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hi all,
I am a beginner with both TIs' u-Controllers and forums, so if the topic has been already discussed, I am sorry in advance for the repeated request.
Following…
Part Number: TMDSCNCD28P65X Tool/software: Hello,
I am working with a custom PCB carrier-card for the controlCARD. On the PCB, each of the 5V pins on the 180-pin HSEC connector is connected to an external 5V source.
Is it safe to power the controlCARD…