Part Number: TMDSCSK8127 Other Parts Discussed in Thread: IPNC-RDK-CSK , TMS320DM8127 I work with TMDSCSK8127 board and use IPNC-RDK-CSK (3_9_1) I need to change and read PLLSS (and any other) register values from the terminal
As I understand, linux_pr…
Part Number: TMS320DM8127
Hi, I'm using camera starter kit in full feature mode with AR0331 sensor. How can I manually set exposure time bypassing 2A engine during RTP streaming (2A disabled in web interface) ? I Board is new for me and all documentation…
Part Number: TMDSCSK8127 Tool/software: Linux Looking to create a simple Linux application for the 8127. I have the IPNC application building and executing on the TMDSCSK8127 board. The tools are provided to build and create the IPNC application. This…
Part Number: TMDSCSK8127 Tool/software: Linux I have an application that does not allow an SD Card to be configured or installed on the Evaluation board. I require the ability to place u-boot into NAND flash. Through contact with TI support and the forum…
Part Number: TMDSCSK8127 Other Parts Discussed in Thread: TMS320DM8127 Hi, I'm new to TMDSCSK8127 .
The start kit (or sd card) seems to have a problem.
I followed the enclosed Quick Start Guide but I saw the "CCC...." in teraterm.
Saw a…
Part Number: TMDSCSK8127 Other Parts Discussed in Thread: TMS320DM8127 I have an issue with the TMS320DM8127 Camera Starter Kit (CSK). The system seems to boot up properly, but I can't seem to get the camera to be shown either on the display attached directly…
Part Number: TMDSCSK8127 Tool/software: Code Composer Studio Is there Code Composer Studio support for the 8127 Target Platform?
If so, are there any examples that can be used to initialize and bring up the platform independent of Linux?
Simple “Hello…
Part Number: TMDSCSK8127 Hello. I'm new to TMDSCSK8127.
The start kit (or sd card) seems to have a problem.
I followed the enclosed Quick Start Guide but I saw the "CCC...." in teraterm.
Here is the log. What's the problem?
________…
Part Number: TMDSCSK8127 Tool/software: Code Composer Studio Can someone explain the procedure for connecting to the DSP using the on-board USB emulator provided with the DM812CSK?
Using CCS version 5.5
CCS Target platform configuration: Connection=XDS100v2…
Part Number: TMS320DM8127 Other Parts Discussed in Thread: TMDSCSK8127 , , DM388 Dear Experts
My customer would like to buy DM8127 EVM TMDSCSK8127 from our website but got below alarm.
It seems this EVM is not available.
Is there any alternative solution…