Part Number: TMDSCSK8127 Tool/software: Linux Have custom hardware that is designed around the 8127 and uses an Atmel SPI Flash part for u-boot.
Looking to add ATMEL spi flash support to the spi-flash-writer utility and u-boot .
I have attached a snippet…
Sang,
Do yo use TMDSCSK8127 Evaluation Module?
DM8127 camera starter kit (CSK) contents:
• TMDSCSK8127 module
• CSK carrier card
• Camera module (LI-CAM-AR0331-324-1.8) with FPC cable
DM8127 CSK comes with XDS100v2 on board emulator, located at…
Hi,
>>i have tried to apply a new template to this device (namely FT222H). Could this be the reason for all of my trouble ?
Without much further details, I would guess this is the source of the issue.
Your FTProg screenshot indicates the device…
Hi,
Our team has only tested the DDR3 used with the DM8127 CSK
www.ti.com/.../tmdscsk8127
We don't have any recommendations for other DDR3 memories
thank you
Cesar
Hi,
Please take a look at some newer boards.
www.ti.com/.../tmdscsk388
www.ti.com/.../tmdscsk8127
One thing to keep in mind is that the sw development for these platforms is completed and only limited support will be provided
e2e.ti.com/.../66041…
Part Number: TMS320DM8127 Tool/software: Linux
This is the Camera Kit, TMDSCSK8127: I still have problems booting into u-boot prompt. Only 'CCCC..' appears on screen.
After rebuilding u-boot, ... with ipnc_rdk-3.9.1, I don't see 'CCC..' on…
Hi,
The DM8127 RDK has an optimized software architecture. It does not use V4L2 framework.
Before purchasing the CSK EVM I encourage you to download the Software Package. It includes a test report of all the use cases tested.
www.ti.com/.../TMDSC…
Jaison,
Do you use the same DDR3 chips for DM8127SCYE3 and DM8127BCYE3?
For example in DM8127 Camera Starter Kit, DDR3 chips are MT41K256M16TW-107. In the TMDSCSK8127 module, two 4-Gb (256Mx16) DDR3L chips (MT41K256M16TW-107 [backward compatible to…
Part Number: IPNC-RDK-CSK Tool/software: Linux Could you help me ? Thank you!
My question:
1, I have a TMDSCSK8127-CSKCC-BNDL buyed from ti. I have a camera module(LI-CAM_AR0331-1.8) and a TF card from Ti dm8127-CSK.
2, I powered up the dm8127 board …