Note that I am not an expert on this board. However I noticed some of your jumper and switch setting are different than mine. Try matching mine exactly.
Part Number: TMDSEVM5517 Hello,
As I was working on TMDSEVM5517 evaluation board, everything was working fine with few of my basic example codes. And now here I'm stuck on configuring OLED with the evaluation board, there is no source or documentation…
Part Number: TMDSEVM5517 Hi E2E, Our customer is looking for the PCB files, schematics, technical reference, BOM of TMDSEVM5517. The link in the previous E2E post is no longer available. Regards, Carlo
Part Number: TMDSEVM5517 Hi,
my customer got TMDSEVM5517 but it didn't include 5V power supply (AC adapter). They would like to get the 5V power supply.
Could you tell us what ampere the EVM is needed? We would appreciate it if you show us the parts…
Part Number: TMDSEVM5517 Hi,
I am willing to enable two codec in EVM5517. I modified sample code name "CSL_I2S_AudioCodec_DMA" from CSL example code by setting SEL_I2C_S0 = 0 and SEL_I2C_S1 = 1 via ioExpander_Write and only define INSTANCE0_I2S…
Part Number: TMDSEVM5517 Yesterday, while I was working on C5517 evaluation board (TMDSEVM5517), there has been some smell of burning from the board. I’ve immediately turned it off.
I switched it on today, but the on-board USB emulator fails in…
Part Number: TMDSEVM5517 Hi,
I am trying to do a POC to transmit and receive data between EVM5517's I2S0 and LAUNCHCC3220 I2S port. EVM5517's I2S0 is set as Slave mode while LAUNCHCC3220 I2S port is set as Master mode with 48kHz sampling rate.…
Part Number: TMDSEVM5517 Tool/software: Code Composer Studio I would like to connect to the target in realtime mode, in order to get access to the CIO console when booting from flash. I've seen that, this can be achieved by enabling realtime mode from…
Hi Baskar,
The following C55xx parts have the TI HWAFFT: C5535, C5515 and C5517. Among them, the C5517 has the best performance. There is a C5517 EVM available on ti.com:
TMDSEVM5517 Evaluation board | TI.com
The HWAFFT example is in
dr-download.ti.com…