Hello U-SK,
The reference design is for 4 mics.
So if you want to do 6 mics, a couple of suggestions:
1) Disable DRC to see if the problem goes away.
In bf_asnr_mss_vau.h uncomment #define STATIC_BF so that static beam forming is enabled.
This will disable…
Hi Ming,
Thank you,
The program build was successful when I mapped VC5505_I2S.cmd file as the linker command file.
but can we load and test the bf with TMDSEVM5517 evaluation board because the target device is C5517.
Thanks,
Hima Bindu
Part Number: TMDSEVM5517 Other Parts Discussed in Thread: TMDSEMU110-U Tool/software: Code Composer Studio Hi TI suppoters,
I tried to connect embedded XDS100 JTAG on EVM5517 to an external C5517 processor.
This processor is already supplied power and…
Part Number: TMDSEVM5517 Other Parts Discussed in Thread: TMS320C5517 Tool/software: Code Composer Studio I'm am running an example program (CSL_McBSP_Interrupt_Example, on CCS8.3.1) and want to modify a register value while the program is stopped at a…
Part Number: TMDSEVM5517 I just completed the C5517 EVM Quick Start Guide and have verified that all the switches are in the correct positions. However, when I power up the board nothing happens (besides the power LED coming on). Based on step 9 ("Navigate…
Hi YR C
Are you still stuck and looking for response from Mark? Looks like Mark has been tied up.
Can you explain your end use-case a bit and time lines for production etc?
Regards
Mukul
Part Number: TMDSEVM5517 Other Parts Discussed in Thread: TIDA-01470 , Tool/software: Code Composer Studio Hello,
I have been following along with the TIPED-0077 reference design that combines the TMDSEVM5517 and the TIDA-01470 PCM1864LMBEVM. I have created…
Part Number: TMDSEVM5517 Tool/software: Code Composer Studio In the C5517 EVM Quick Start Guide they mention that the C5517 EVM DSP board includes on-board emulator (XDS510 class). I can't find that as a valid option when I chose a new CCS project.…