Dear Customer,
Sorry for the delayed response.
Please visit the links below for the emulator connection issues.
https://software-dl.ti.com/ccs/esd/documents/ccs_custom_target_config.html
https://software-dl.ti.com/ccs/esd/documents/ccsv7_debugging_jtag_connectivity_issues…
Dear Customer,
Sorry for the delayed response.
For flashing the images into EVM, please visit the Processor SDK RTOS guide : http://software-dl.ti.com/processor-sdk-rtos/esd/docs/latest/rtos/index_how_to_guides.html#flash-bootable-images-c66x-k2h-k2e-k2l…
Part Number: TMDSEVM6657 Hello.
Now I'm trying to make QPSK to 16x16 IFFT , So I put even side to real, and odd side to imag.
and adjust all of Scale.
But Output signal's is not corret with matlab function.
eg. input = [1 -1 1 -1 1 -1] (= (1-1j…
Part Number: CCSTUDIO Hi Team,
Customer encountering error in our CCS. Please see image below.
According to customer, they already installed the package but problem is not solved.
Thank you.
Regards,
Maynard
Part Number: TMDSEVM6657 Recently, I recompiled IBL under MCSDK_2_01_02_06. I compiled with I2C_BUS_ADDR of both 0x50 and 0x51.
make evm_c6657_i2c ENDIAN=little I2C_BUS_ADDR=0x51
make evm_c6657_i2c ENDIAN=little I2C_BUS_ADDR=0x50
The two result are…
Part Number: TMDSEVM6657 Other Parts Discussed in Thread: TMS320C6657 Hi,
I bought the TMS320C6657 Evalution module. I followed the procedure from quick guide setup during DHCP it is get failed. I attached the putty image kindly verify and guide me to…
Part Number: TMDSEVM6657 Hello TI Team
We use the TMDSEVM6657LS evalution modele (with integrated xds2000 emulatour) platform to run the HUA OOB demo, and follow the steps 1-5 in the quick setup guide, but the ip address is not obtained. Re- Press the…
Hi,
CS0 is connected to NOR flash. CS1 is connected to FPGA. With the current 6657 EVM assembly, there will be conflict if the customer wants to connect another SPI device on the expansion connector. There is a SPI clock buffer on the EVM that has series…
Part Number: TMDSEVM6657
Hello once again,
I am trying to work with TMDSEVM6657 board. After working correctly for some time already, now when I tried to power it, SYS_PG1 LED is not active anymore, as well as D1 and D2. only D17 is glowing. Also when…
Part Number: TMDSEVM6657 Tool/software: Code Composer Studio Hello everyone,
I am working with TMDSEVM6657 and I am trying to execute the edma_test.c from the example folder. However after building I am getting the error: could not open source file "ti…