Part Number: TMDSEVM6670 Hello!
I need to make an experiment with TMDSEVMC6670 which was purchased a decade ago. Nothing left from original package besides the board and power supply. I had a hope I could refresh my memory about DIP switches in EVM's…
Part Number: TMDSEVM6670 Hello We run tcp3dExampleProject example for evm 6670 in LTE mode. This example loads 6 LTE blocks into the decoder and starts the decoding process. At the end of the decoding, an interrupt is issued and the input data is compared…
Part Number: TMDSEVM6670 Dear team,
Our customers want to see the datasheet or user guide of TMDSEVM6670LE and TMDSEMU560V2STM-UE.
But we cannot find on the TI website.
Would you please help to provide to me??
Thank you very much.
Part Number: TMDSEVM6670 Tool/software: Code Composer Studio Hi:
The LED on our XDS560V2 is out of control and XDS560V2 can not connect to our PC.
We have already ask these question before. However, there is no reply.
https://e2echina.ti.com/question_answer…
Part Number: TMDSEVM6670 Tool/software: TI-RTOS My project is constructed in the basis of two cores. NDK project runs on core0 and FFTC runs on core1. From the perspective of time, it takes NDK 1ms to receive a fixed length of data during each iteration…
Part Number: TMDSEVM6670 Tool/software: TI-RTOS Hi ,
I am using the examples codes provided by Ti for Advance Event Trigger (From below link)
gforge.ti.com/.../
I was able to import the example project for my device i.e 6670 keystone 1, but i m not getting…
Part Number: TMDSEVM6670 Tool/software: TI-RTOS Hello team,
during the development of my project I've met one question which seems uncertain to me. It's about TIMI0 and TIMI1 pins in C6670 processor.
You write in your documentation: http://www.ti…
Part Number: TMDSEVM6670 Hello team,
I have found DDR memories you put on Starter Kit, i.e. K4B2G1646C-HCH9 (DDR3-1333 (667MHz @ CL=9, tRCD=9, tRP=9)) end of life (EOL):
Why do you put EOL elements on Starter Kits available to purchase?
Nevertheless I…
Part Number: TMDSEVM6670 I have use the method which ti gives us to boot DSP from PC by EMAC.The DSP can start up successfully.Now we need to transmit the UDP packets by embedded device.It is really no difference between the PC packet and the embedded…
Part Number: TMDSEVM6670 Tool/software: TI-RTOS Hello team,
I am trying trying to generate an interrupt at the end of each EDMA transfer, unfortunately with no success - the interrupt doesn't occur.
What I have already done is an EDMA transfer implementation…