Part Number: TMDSHVMTRINSPIN I have one of the Marathon 5K33GN2A motors on hand, and was trying to build the Universal Motor Control lab to use this for some experimentation/learning.
I thought I was in luck, as this is one of the motors pre-defined in…
Part Number: TMDSHVMTRINSPIN Other Parts Discussed in Thread: CONTROLSUITE Hi Experts,
Our customer is doing motor control with our inverter TMDSHVMTRINSPIN. He needs the Shunt resistor value used for the current shunt resistance and the current sense…
Part Number: TMDSHVMTRINSPIN
We are facing problem while running the serial port on control card JTAG Interface while running it on TMDSHVMTRINSPIN. Serial port is working perfectly good with just control card power supply is ON from its USB port. As soon…
Part Number: TMS320F28069M Other Parts Discussed in Thread: TMDSHVMTRINSPIN , MOTORWARE Hi Team,
Here're some issues from the customer may need your help:
1. During the lab5c experiment with the TMDSHVMTRINSPIN kit, the LD1 on the control card keeps…
Part Number: TMS320F28069 Hi team,
Here's an issue from the customer may need your help:
In Lab5b, during the test it was found that the speed reference value for PID control of the speed loop was 52707179 and was constantly changing:
But the customer…
Part Number: TMDSHVMTRINSPIN Hello Dear,
I am using Hardware TMDSHVMTRINSPIN and Software Instaspin lab's. I am connecting servo motor with it.I have several questions about it but here the motor parameter
#define USER_IQ_FULL_SCALE_FREQ_Hz (USER_MOTOR_NUM_POLE_PAIRS…
Analogics Rnd Solar said: Can you please provide the est_run() and est_getfm_lp_hz() definitions for our clarification.
You can find the definitions in the "est.h", and refer to the example lab to call the functions.
Analogics Rnd Solar said…
Part Number: TMDSHVMTRINSPIN Hello Dear,
We are give AC input to the circuit and connected nothing with it, also boost PFC also by passed. But the Bridge DC Bus output is increase very slowly Is it normal ? or something fault in the circuit.
Hi, i had a chance to get started with the kit again. I started with lab 1 and i was able to get everything working and blink the led on the control card and was able to change frequency of blinking... The lab also mentions there should be 50% duty pwm…
Part Number: TMDSHVMTRINSPIN
I am trying to make sensorless control work properly for my motor. I am working with TMDSHVMTRINSPIN HVKIT yellow board and TMDSCNCD280025C control card to run an SMPMSM motor which is 30kW and 120,000RPM and following these…