Part Number: TMDSIDK572 Hi,
We have downloaded an RT-Linux SDK. It has a binary file (.bin). We have a windows machine .What is the Procedure to mount this RT-Linux Bin onto the sitara processor.
Please guide on the same.
Part Number: TMDSIDK572 Hi,
Please check the attached image file.I have installed the Linux-RT SDK of AM572X version 8 which is a bin file. How to embed that file into the sdcard and check with the eval kit hardware. Please clarify.
Also what's the…
Part Number: AM5729 Hi Experts,
Seeking your assistance on this query from Cx:
I'm trying to build the SDK as described here:
https://software-dl.ti.com/processor-sdk-linux/esd/AM57X/08_02_01_00/exports/docs/linux/Overview_Building_the_SDK.html…
Part Number: TMDSIDK572 I have the board "TMDSIDK572 EVM". With the help of the PROCESSOR-SDK-LINUX-AM57X (Version 08_02_01_00) I want to build the image "tisdk-default-image". I have performed all the steps described in the section "Download and Install…
Part Number: TMDSIDK572 Other Parts Discussed in Thread: AM5729 , AM5728 , DRA752
Fullscreen
4745.boot.log
Download
1 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file boot.scr…
Part Number: TMDSIDK572 Hai,
We are just getting started with TMDSIDK572, Please help me to understand or Resolve the following Questions:
1-> For using The feature on board Debugging(Xds100v2) Do we need to Jumpers on EVM board, if Yes Which jumpers…
Part Number: PROCESSOR-SDK-AM57X Other Parts Discussed in Thread: TMDSIDK572 Hello everyone!
I use the board "TMDSIDK572" (AM572x Industrial Development) and the "TI PROCESSOR SDK LINUX for AM57X " for my developments.
After many tries and some corrections…
Part Number: TMDSIDK572
Performed the following steps:
Enabling Android Automotive on Your TI Development Board
When performing these steps from 3 to 5, the following are the outcomes:
3. Open a terminal debugger to view console output from the…
Other Parts Discussed in Thread: AM5728 , TMDSIDK572 Hello!
I use the evaluation board "TMDSIDK572" (so with the SoC "TI AM5728").
I'm using CCS v12.2.0.00009 with installed "Sitara Device Support v1.6.3.
I have now created a CCS Project for C66…