Information about the Experimenter Kit can be found in controlSUITE and C2000Ware. You will need to install either one, if it is not already installed on your computer.
In C2000Ware: C:\ti\c2000\C2000Ware_<version>\boards\PeripheralExplorerKits\TMDSPREX28355…
Hi Nipun, The launchPAD/boosterPACK and controlCARD/DockingStation are two hardware ecosystems for experimenting and writing software with the C2000. The launchPAD is typically slightly more low-cost oriented whereas the controlCARD would be a bit more…
Nedzad, Firstly, if you buy the Peripheral Explorer Kit (TMDSPREX28335), it will come with the F28335 Delfino controlCARD as you mention. It is certainly possible to put a F28069 controlCARD (TMDXCNCD28069) into this Peripheral Explorer kit and you will…
Khaled, Have you attached any additional hardware onto the Experimenter's Kit? If not I would recommend attaching a CAN transceiver and termination resistors (max 2 in the network) as in the Peripheral Explorer hardware: \controlSUITE\development_kits…
Hi Brett,
I have read the contents used in TMDSPREX28335 using Mprog utility and replicated the same .ept file on my board. The board is being recognized as the development board works. Please find the screenshot of my device manager.
and my board…
Example_2833xECanBack2Back uses self-test mode and will not need any transceivers.
If you use the C2000 Peripheral Explorer Kit : TMDSPREX28335 : There is an onboard CAN - Tranceiver for CAN-A
If you use the TMS320F28335/C28343 Delfino Experimenter…
That is probably too much data to fit in the RAM. I would recommend logging to external memory, such as the EEPROM you mentioned. You can check out the software for the Peripheral Explorer Kit to see how this can be done using SPI.
http://focus.ti…
Murat, We do not have any F28335-based tools that are built around SYS/BIOS. However, it is certainly possible to start working with SYS/BIOS on the F28335. The following link may be helpful: http://e2e.ti.com/support/microcontrollers/tms320c2000_32-bit_real…
Other Parts Discussed in Thread: TMS320F28335 I try to use the control suite examples for TMS320F28335. When I debug the active projects, it is given an error as " This project was created using a version Code generation tools that is not currently installed…