Other Parts Discussed in Thread: CC1125 , CC1121 , TMDX5515EZDSP , CC1120 Hi all,
I need to develop a device to transfer audio data from two points 100 meters apart each other.
Audio data have a bitrate of 64kbps (compressed by opus codec).
Except for 2.4GHz…
Other Parts Discussed in Thread: TMDX5515EZDSP According to SPRUFP1 p. 19 I shuld be adble to modify the ADCCLKDIV register in a range 1-32768. But when I load my code on my TMDX5515EZDSP here what I see:
I am only able to change the value from 0 to…
Other Parts Discussed in Thread: TMS320C5515 , TMDX5515EZDSP One is EZ430RF2560,which is needed for EMG+IMU board developing. It contains MSP430 and Bluetooth module.
The other is TMS320C5515 eZdsp USB stick(DSP), which is the tool for sound recording in U…
Other Parts Discussed in Thread: TMS320C5515 , TMDX5515EZDSP Hey TI team,
I started to work with the TMS320C5515 FDK. Im a beginner in the DSP-progromming world and have no Idea where I have to begin. I use ccsv5 and my operating system is windows 7 Following…
Other Parts Discussed in Thread: TMDX5515EZDSP I'm using TMDX5515EZDSP. I am able to configure GPAIN1 Channel 3 to perform a proper ADC conversion using API functions. When I only change ADC settings to perform the same on the Channel 2 nothing happens…
Other Parts Discussed in Thread: TMDX5515EZDSP I've got the new TMDX5515eZDSP but there are no schematics or other documentation in addition to the quick start guide. Where can I found more datasheets? Already checked the Spectrum Digital site but it was…
Other Parts Discussed in Thread: TMS320VC5502 , TMDX5515EZDSP Hello,
I am working with low power TMS320C5502. I am a control engineer and implementing Neural Network for controlling and system identification.
Does Texas Instruments support me to develop…
Other Parts Discussed in Thread: TELECOMLIB , TMDX5515EZDSP Hi, colleagues,
my customer is in search of a hardware+software solution of an angle audio application: the system should hear only the sound from an hearing zone formed by a beam of 30 degree…
Other Parts Discussed in Thread: TMDX5515EZDSP I recently purchased the TMDX5515EZDSP USB Stick which came with a version of CC4. After installing, CCS4 asked if I wanted to download and install updates, to which I answered yes. The download and first…
Other Parts Discussed in Thread: TMDX5515EZDSP The second question is why I cannot set channels 0 through 2 on GPIO0 for converting by SAR ADC input voltage? The value is always about zero. All the other channels work flawless. Could someone please provide…