Part Number: TMDSEVM6657 Other Parts Discussed in Thread: TMS320C6657 , TMDXEVMPCI Hello,
I started to design with TMS320C6657CZHA25 device for FPGA interface.
I am considering PCIe bus : TMS320C6657CZHA25(PCIe endpoint), MPSOC(PCIe rootport).
For performance…
Hello Rex,
So to clarify, if there's no breakout card to support PCIe for this board, how is PCIe supported? Using the 170 pin B+ style AMC interface?
I found that TI offers this: www.ti.com/.../TMDXEVMPCI
Would this work for the EVMK2EX?
Hi,
The C6657 EVM can be converted to PCIEx4 connector via http://www.ti.com/tool/TMDXEVMPCI , this is an AMC to PCIE adapter. For the error injection card, it is PCIEx16. I am not sure if there any cables to connect them together. We typically buy such…
Hi,
We have Linux PCIE driver example for C6678. It is under pdk_c667x_2_0_x\packages\ti\boot\examples\pcie. We don't have Windows PCIE driver.
The adapter: www.ti.com/.../TMDXEVMPCI
Regards, Eric
Part Number: TMS320C6678 Other Parts Discussed in Thread: TMDXEVMPCI Hi all,
We are trying to use C6678 as Route Complex (RC) and we are looking for a compatible PciE back-plane.
Is there a specific back-plane that we should use ? We are using PciE Gen…
Part Number: TMS320C6657 Other Parts Discussed in Thread: TMDXEVMPCI Hello,
I am planning on purchasing the TMDXEVMPCI support board to connect with the PCIe peripheral on a C6657 EVM Board (TMDSEVM6657L). I had a question about the PCIe output from the…
Part Number: EVMK2H Hi there,
I am trying to run the PCIe example included with the processor SDK for the K2H EVM. I have two EVMK2H demo boards, and two of the RTM Break-out cards for the Keystone II EVM. Once I have built and loaded the PCIe demo on…
Part Number: TMS320C6678 Hi,
I have been testing the TMX320C6678 evaluation board assembled in TMDXEVMPCI adaptor-card, in a PC. i followed the Desktop SDK Hardware setup guide:
and the PCIe device wasn't enumerated by PC. i checked the PC's BIOS setting…