Part Number: TMDXIDK5718 Other Parts Discussed in Thread: ISO1641 Hello!
We are using TI-RTOS to communicate over I2C. We are using I2C1 to communicated with an ADC through an ISO1641 isolator. We are observing a condition where the I2C driver enters…
Part Number: TMDXIDK5718 I am currently using TFTP boot. To the image I started with, which was built with TI SDK (yocto built), I added a few packages (e.g. pyscard) directly on the target by building them on the target using source codes (I found the…
Part Number: TMDXIDK5718 Hello,
I'm encountering an error where if I attempt to attach with a XDS110 Debugger I see the following Error Output below. This issue primarily occurs if the Processor has already been flashed with a QSPI Image that it is booting…
Part Number: TMDXIDK5718 I am running tisdk-base-image on TMDXIDK5718. Can you please describe a procedure that enables all six ethernet ports available onboard. No matter what i try to enable them, only one that actually works is etho - and that is by…
Part Number: TMDXIDK5718
Hello,
Hello, I am trying to install the most updated version of docker on my TMDXIDK5718, currently the version that is installed is the following: DOCKER_VERSION = "19.03.8-ce", how can I update the version?
Part Number: TMDXIDK5718 I'm going through the procedure described in
1.2. Building the SDK.
It mentions Cross-Compile Toolchain requirement and describes the following:
Download the toolchain compilers from the links provided in the SDK release page…
Part Number: TMDXIDK5718 I have questions regarding Quick Start process for Building the SDK.
Host is Ubuntu 22.04.3 LTS,
Per the instructions given in Quick Start, executing the apt-get step produced the following error:
peterh@peterh-Surface-Laptop…
Part Number: TMDXIDK5718 Hi.
I created and have been using the default linux bootable image provided in the SDK. It comes with Python 3. In order to continue evaluation, I need to get additional packages (i.e. sudo apt install). It appears, however, The…
Hi Peter,
Sorry for the delay in response.
Are you able to bring up the interfaces using ifconfig with the following command?
command : "ifconfig eth1 up"
Regards, Tanmay