Part Number: TMDXRM57LHDK Tool/software: Hello,
We are using the TMDXRM57LHDK reference board and wanted to be able to read/write to Bank 7 of flash using the FEE drivers. Are there any additional steps necessary in HalCoGen to be able to allow using…
Part Number: TMDXRM57LHDK
Hello,
We are using the Hercules TMDXRM57LHDK Dev Kit Rev E. Where can I find the info for what populated pins for SCI and SPI Schematic/Manual we can access on your Hercules board? Specifically SCI2, SCI3, SPI1 and SPI5 right…
Part Number: TMDXRM57LHDK
Worked on an RM57 Launchpad board. Was able to connect to it in CCS via the XDS110 debugging USB connection. I am trying to setup a project on the RM57 HDK Hercules platform as well. I am also using the XDS connection as the…
Hi Gloria,
Icgoo Icgoo said: We tested all the J4 pins and determined that R291 should be shorted.
Yes, to get 1.2v from U35 regulator R291 should be shorted and R293 should be open.
Icgoo Icgoo said: Please help determine if this is a defect in the part…
Part Number: TMDXRM57LHDK Hi All
Please can you let me know what format the PCB layout is for spnr038.zip. I have tried to import RM57_hdk_reve.brd into AltiumDesigner AD22 as an Eagle design but it does not recognize the file. I have also tried to open…
Part Number: TMDXRM57LHDK Hi, My customer is debugging SafeTI Diagnostic library demo code on RM57L HDK. According to below thread, after _SL_Kickoff_STC_execution(), CPU should be reset: https://e2e.ti.com/support/processors-group/processors/f/processors…
Part Number: TMDXRM57LHDK Hi, My customer is trying to connect TMDXRM57LHDK with CCS 10.3.1. He got below error at Test Connection.
E _RPCENV_IO_ERROR(-6)No connection:DTC_IO_Open::dtc_io Failed to open i/o connection(xds2xxu:0) An error occurred shile soft…
Part Number: TMDXRM57LHDK Hello,
I created an application in assembly language.
I would like to move an object file in a library.
The library is created with armar.exe.
I insert a parameter in the source file with that syntax:
.global myParam
$myPar…
Part Number: TMDXRM57LHDK Hello,
I use the trace analyzer on a TMDXRM57LHDK development Board since two months without any problem.
But now, When I try to configure the trace analyzer (Hardware Trace Analyzer > Function Profiling) I got the following…
Part Number: TMDXRM57LHDK Hello,
I am attempting to run a test case on the Hercules RM57L843 board through VectorCAST, but the execution seems to crash / hang. I am using a Blackhawk XDS560v2 System Trace Emulator as an external debugger. The code has…