Part Number: TMDXSK437X
How do i run the examples in "ti\starterware\examples"? They do not import like the "MyExamples" (no problem with those). I do see the .out files for these example projects under "ti\starterware\binary". …
Other Parts Discussed in Thread: TMDXSK437X I have the TMDXSK437X and would to control the GPIO pins with Python. The image has Python 3.8, but I don't see any definition on define the IO is there another install I need to do or is everything there I just…
Part Number: TMDXSK437X
Tool/software: TI C/C++ Compiler
I am getting multiple definition errors. One definition is the actual function and the "second" is always a an inline function. I have tried various optimization levels as well as the setting for…
Part Number: TMDXSK437X
Is there any kit for use the J20 signals ?
Whre can I find an edge card with 0.635 pitch adaptation tool ?
Why not used DIMM or PCI pitch on this slot ? It´s unusable feature.
Part Number: TMDXSK437X Tool/software: TI C/C++ Compiler I am getting multiple definition errors. One definition is the actual function and the "second" is always a an inline function. I have tried various optimization levels as well as the setting for…
Part Number: TMDXSK437X Tool/software: Linux Hello;
I bought the Starter Kit TMDXSK437X and some features are not working, speacilly ethernet interface. I want to know with my linux taht came on SD card is up to date. See boot log:
[ 0.000000] Booting…
Part Number: TMDXSK437X
Tool/software: Linux
How to launch a terminal console and configure the IP of ethernet interface ?
I´m using TMDXSK437X, it cames with a SD card that has the Linux system and some demo application, when I select Ethernet settings…
Part Number: TMDXSK437X Tool/software: Code Composer Studio I am getting this warning: Invalid project path: Duplicate path entries found (/MCASP_Audio_evmAM437x_armExampleProject [Include path] isSystemInclude:true includePath:C:/ti/pdk_am437x_1_0_8…
Part Number: TMDXSK437X Tool/software: Starterware Hello,
I have a custom board that is mostly based on "TMDXSK437X" dev kit.
I am trying to locate the existing pinmux_config file for this devkit so I can load it and modify it via PinMux Config…
Part Number: TMDXSK437X Hello,
I have recently bought a TMDXSK437X and on arrival the device would not power on. Is there a fix for this or will I be able to return the board?
Thanks, Broydon