Part Number: TMP102-Q1 Dear Sir,
I would like to get information about obsolescence risk for the TMP102AQDRLRQ1. I mean how long will be this item in production?
BR
Orlando
Part Number: TMP102-Q1 Dear Support Team;
I have a question about accuracy of TMP102-Q1.
The following value In datasheet.
Maximum accuracy : -20℃ to 85℃ ±2℃
Maximum accuracy : -40℃ to 125℃ ±3℃
How many accuracy at -40℃ to -20℃ and 85…
Part Number: TMP102-Q1
Hi Team, The datasheet shows the following two-wire timing diagram. I believe high/low level of the following timing diagram is "VIH_min: 0.7 × (V+)" and "VIL_max: 0.3 × (V+)". Is my understanding correct…
Part Number: TMP102-Q1 Other Parts Discussed in Thread: LMP91000 , TMP102 Team,
Our Customer is working on a Car DVR product and is using TMP102-Q1. They would like to know if we can provide I2C driver for the Temperature sensor TMP102AQDRLRQ1 for Non…
Part Number: TMP102-Q1 Hi, team.
Our customer requesting the actual thermal model for TMP102AQDRLRQ1.
Software is FloTHERM Ver11.3.
Do you have the model?
Best Regards,
Kobayashi
Part Number: TMP102-Q1 Other Parts Discussed in Thread: TMP102 Hi,
Please let me question at Two-Wire timing of TMP102-Q1. Data sheet for TMP102-Q1 (SBOS702C) page12 Two-Wire Timing Diagram is shown in Figure8.
I am at data timing, the time from when SCL…
Other Parts Discussed in Thread: TMP102-Q1 , TMP102 Hi,
I would like to use tmp102-q1 in my LED flash light application. I am planning to place the sensors on the same side of the LEDs and as close as possible to LEDs. As per SBOS702B page 22 (layout guidelines…
Hi Mark,
RθJC(bot) is typically not provided for packages without a thermal pad on the bottom.
Thermal information for the TMP102-Q1 can be found in section 6.4 of the datasheet here: https://www.ti.com/lit/ds/symlink/tmp102-q1.pdf . For understanding…
Part Number: LM73 Other Parts Discussed in Thread: TMP112 , TMP1075 , TMP102-Q1 , TMP112-Q1 , TMP75-Q1 , TMP175-Q1 Hi sir,
It seemed ok, but I still need your confirm.
What should I take care?
thanks.
Alpha
TMP102-Q1 is an auto grade digital temperature sensor which would easily pair with a BLE MCU such as CC2640 over I2C. http://www.ti.com/tool/TIDA-01624
ren