Other Parts Discussed in Thread: TWL6030 , TMP105 , 4430 , 4460 I download the Android pre-built binaries form http://www.omappedia.com/wiki/Android:_Working_with_pre-built_binaries ( L27.12.1-P1 ) .
If I use the MLO(tested) or es2.1_MLO(untested) there is no message…
Other Parts Discussed in Thread: TWL6030 , TMP105 I followed : http://www.omappedia.org/wiki/L27.G.2_OMAP4_GingerBread_Release_Notes and when I save bootargs in minicom, it print out :Type 'y' or 'Y' to Save Environment to NOWHERE.. .
why…
Other Parts Discussed in Thread: TWL6032 , TWL6030 , TMP105 , TMP102 , TWL6040 Hi,
i am using OMAP4460, trying to port android jellybean on this.
i flashed my eMMC by using fastboot, All the images are flashed successfully.
up to x-loader and u-boot came…
Hi,
I am trying to load Android Jellybean 4.2.0 to Blazeboard. Somehow I compiled the image and now I am trying to boot from SD Card. The boot log stops at a point where it shows a message
[62.008911] omap-rproc omap-rproc.1: rproc_loader_cont: failed…
Other Parts Discussed in Thread: 4430 , 4460 Hi,
I have managed to boot 4AJ.1.1 on Blaze from eMMC but I have no success in booting it up on SD card.
I tried two different ways using SD card.
1. Manually partition SD card according to release note guild…
Other Parts Discussed in Thread: 4460 Greetings,
I have the SEVM4430G with the 4460 ES 1.1 processor upgrade from SVTronics. I'm using this drop: http://www.omappedia.com/wiki/L27.IS.2.P2_OMAP4_Icecream_Sandwich_Release_Notes
The kernel is hanging…
Ok, I had to completely delete the ti-processor-sdk-linux-automotive-dra7xx-evm-6.00.00.03 directory and re-install, then right before I ran ./build-core-sdk.sh dra7xx-evm, I modified the iso-codes_4.1.bb with the solution mentioned above, this time it…
Hi,
I tried running " repo sync " in my mydroid directory and compiled again,but still i'm getting the same error.
I made changes to the following files :
1.I added the following lines to mydroid/device/ti/blaze/AndroidProducts.mk
…
Other Parts Discussed in Thread: WL1283 Hi
I am running Android jelly bean 4.2.2 on Blaze Board. As per the release notes i built the compat_wl18xx and copied the modules to the /system/lib/modules, but it failed to load the modules when i booted the board…
I have just received a new TEVM4470G-05-10-00 with processor board 4470 GP ES1.0(D) and main board 2158-004.
It will not display a UI on main LCD (on all android binaries I've tested)
- the uboot splash animation is shown so hw is functional
- if…