Part Number: TMP112-Q1 Hi all,
I would like to know the absolute Maximum Ratings for input current and output current.
Would you please share the data?
Thanks in advance.
Best regards, Toshi
Part Number: TMP112-Q1 Hello team,
I have a question about TMP112-Q1 SDA/SCL pins during Power OFF (V+ =0V). Do TMP112-Q1 SDA/SCL pins become Hi-Z at V+ =0V? If so, MCU can communicate with other I2C devices at same I2C line. Would you please advise? Best…
Part Number: TMP112-Q1 Other Parts Discussed in Thread: LM50-Q1 , LMT87-Q1 Hi
We need TMP112AQDRLRQ1 FMEDA date for ISO26262 certification, can you provide ?
Part Number: TMP112-Q1 Hi team,
I have a question about a definition of the spec in TMP112-Q1 datasheet page16.
If the conversion rate is set to 4Hz(default), How long is the Delay in Figure14?
4Hz=1/250ms,
I would like to know if 26ms of conversion time…
Part Number: CC1310 Other Parts Discussed in Thread: TMP112 , IC:CC1310F128RHB
Use case :rfEasyLinkTX....nortos_css
my demo RF PA SKY66115 ,LDO controls the SKY66115 power supply, LDO EN is IOID_9.
IOID_8 is tmp112 power
my demo mcu use pin IOID_2, IOID_1 ,IOID_9…
Part Number: TMP112-Q1 Hi,
I used this device on my project. On SCL, SDA and ALERT pins I put a 5kohm Pull-Up through 3.3V, the V+ pin connected dierctly to 3.3V, ADD0 and GND pins connected to 3.3V's GND and between 3.3V and GND I put a 100nF capacitor…
Part Number: AWR2243 Other Parts Discussed in Thread: TMP102-Q1 , TDA2 , , TMP102 , TMP112 , IWR6843 We notice that there are dedicate temperature sensors (TMP102-Q1) on both 2-chip and 4-chip cascading image radar reference designs.
We are wondering if it…
Part Number: TMP112-Q1 Hi!
We want confirm the current consumption of TMP112-Q1 at 125℃.
<Question> 1.How much is the shutdown current at 125℃? (TEST CONDITIONS :Serial bus inactive) 2.How much is the active quiescent current during conversion at…
I talked with our development team. More detailed answer below:
All qualification plans for the TMP112-Q1 are in compliance with AEC Q100 and AEC Q006. Those test included on the TMP112-Q1 are:
Final test outlier procedures
Auto visual inspection
Design…
Ranger,
The FIT data available to provide for the TMP112 is below. Keep in mind this is for the TMP112AQDRLRQ1 orderable. ( TMP112-Q1 )
Component Failure Rates per IEC TR 62380 / ISO 26262 Part 11
Total FIT Rate- 4
Die FIT Rate- 2
Package FIT Rate- 2
…