Part Number: TMP112 Other Parts Discussed in Thread: TMP113EVM Tool/software: Hi,
I'm using the EVM112EVM, successfully connecting to the device with the TI Web software.
I need to save a long log, of 30 min or similar.
When I press "SAVE START…
Part Number: TMP112EVM Other Parts Discussed in Thread: TMP102 , TMP112 , Hello Expert,
My understanding for TMP112 is software and drop-in compatible device against TMP102. Then, I'd like to know about whether we can use TMP112EVM's USB controller…
Part Number: TMP112EVM Hi Team,
I tried to make sure that GUI recognize device connect after splitting in two.
* 3.3 V and GND of U6 side are connected to DC 3.3 V Power supply
But, GUI said that I failed to connect to device.
Splitting TMP112EVM…
Part Number: TMP112EVM Other Parts Discussed in Thread: TMP112 , TMP390 , TMP392 Hi, team,
My customer is evaluating TMP112EVM for a new project. TM=1 for interrupt mode, only this bit of configuration register was set, other bits were using default…
Other Parts Discussed in Thread: TMP112EVM Hi,
In the document, SBOU144–August 2014, of TMP112EVM Documentation, its mentione din Page 20 that the connector J1 is 851-43-050-20- 001000 which is Connector, Socket 50-Pin .050 R/A
In the schematic…
Part Number: TMP102 Other Parts Discussed in Thread: TMP112EVM , TMP112 Hi team,
My customer is considering TMP102.
What is the recommended EVM for TMP102?
Should it be TMP112EVM?
Is there any modification needed to evaluate TMP102 on TMP112EVM…
Hi Atsushi-san,
You're referring to page 11 of the datasheet:
Bit D0 of byte 2 indicates normal mode (EM bit equals 0) or extended mode (EM bit equals 1), and can be used to distinguish between the two temperature register data formats. The unused…
Other Parts Discussed in Thread: HDC2080EVM , TMP112EVM Hello! I am wondering, what does it mean when it say "evaluation module"(EVM)? Like AWR1642EVM, HDC2080EVM, TMP112EVM, TDC1000-TDC7200EVM? Thank you.
Dear S Gokula Krishna -
Welcome to E2E and thanks for posting!
Neither the TMP116 nor the TMP112 are infrared temperature sensors, I can confirm that for you.
If your project is about that specific type of sensing, as the TMP007 is discontinued…