Part Number: TMP116 Hello,
My customer would like to know if TMP116AIDRVT can pass the ultrasonic cleaning process after manual mounting on PCB.
Please advise, thanks.
Part Number: TMP116 Hi,
With TMP116 temperature sensor driver we are able to read the raw value of temperature, Please provide if any formula available to extract actual temperature from obtained raw value.
Thanks,
Nikhil K
Part Number: TMP116 Does TMP116 support reading/writing multiple registers in a single I2C transfer? Many I2C devices allow the base register to be selected and additional registers accessed by clocking additional bytes.
For example: If I start read…
Part Number: TMP116 Dears,
We are using digital temperature sensor chip TMP116AIDRV, one IIC bus is mounted with two temperature sensors, STM32F405 is used to drive. IIC is simulated by IO port, IIC pull-up resistance is 4.7K, 100K clock is used, and…
Part Number: TMP116 Hi Expert,
My customer are using C2000 to communicate with TMP116 by I2C, ADD0 pin is connected to SDA, seem from the I2C waveform, C2000 send correct device ID waveform which is 1001010x, and command 0x0F, but TMP116 send back 0xffff…
Part Number: TMP116 Hi,
(1) Is there a possibility that TMP116 will hang or lose communication due to static electricity? If a hang occurs, is there a way to recover?
(2) Will the value of the internal register of TMP116 be rewritten due to static…
Part Number: TMP116 Hi Team,
The other thread below shows that the temperature drift of TMP116 equates to 10-15 years at 25C. Our customer would like to know the temperature drift after 6 years at 60C. Can you please share the formula/graph to calculate…
Part Number: TMP116 Other Parts Discussed in Thread: TMP117 Is there a higher precision I²C interface temperature sensor chip (precision ≥±0.1℃) than TMP116. Requires easy supply from mainland China.
Part Number: TMP116 Hi Team,
Our customer would like to know the maximum Output Low Current Rating for SDA Output Logic Low level. According to our customer,
We are using TMP116N Digital Temperature Sensor in a defense application. A contractor…