Part Number: TMP117 Based on our current layout, the IC's top side is oriented toward the skin. However, the TMP117 guidelines state that the bottom side face the skin for optimal thermal response.
Will our current component placement affect the accuracy…
Part Number: TMP117 Other Parts Discussed in Thread: CC2640R2F , CC2640 , , ASH , TIDA-01624 , TMP119 , UNIFLASH , USB2ANY Hi Everyone,
Hope you guys are doing well.
For the past one month I was trying to interface TMP117 body temperature with CC2640R2F…
Part Number: TMP117 Hi,
Our TMP117 sensors are embedded in a finished product, so we can't physically inspect the package marking. We'd like to verify them via the factory-programmed Unique ID (EEPROM1/2/3).
Readings:
Device 0x48: EEPROM1=0x4F6D…
Part Number: TMP117 Hi,
I am trying to interface the TMP117 temperature sensor with an ESP32 DevKit using ESP-IDF. The sensor is on a SmartElex breakout board. I am getting a timeout error and the I2C scan finds no devices on the bus.
Setup:
MCU…
Part Number: TMP117 Other Parts Discussed in Thread: TMP118EVM , TMP118 I am looking at the option of mounting the TMP117 BGA chip directly to flex PCB. My concern is about long term reliability as the chip can be a bit fragile and I feel intuitively…
Part Number: TMP117 Dear TI support,
we want to use two tmp117 in one device and set them up to continuous conversion (CC), 4s, no average. In a PoC we see, that the 4s interval both sensors deviate from each other over the time. I already searched…
Part Number: TMP117
11.TMP117 is applied to the instrumentation project.4 pieces per board, 10 boards for 1 system.Occasionally, during operation or shortly after power-on, the temperature of this chip can reach 60℃ or 80℃.The I2C communication works…
Part Number: TMP117 Other Parts Discussed in Thread: TMP110 , TMP112 Hi Team,
my customer is evaluating TMP117 in smartphone and they are wondering if we have linux driver code for TMP117, thanks.
BRs.
Frank Cai
Part Number: TMP117 Dear TI Engineer,
One of our smartwatch project is using the TMP117MAIDRVR to monitor the human temperature, and the electrode pads in contact with human skin are made of steel. We would like to confirm the thermal conductivity…