Part Number: TMP123 Tool/software: Hi Team,
Please help to provide datasheet , MSL , Body marking , Tape width , Tape pitch and pin 1 orientation for below MPN.
TM4C123GH6NMRT
TM4C123GH6NMRT7
TLV3701CDBVTG4
TMP123AIDBVRG4
TMP123AIDBVT
…
Part Number: TMP123 Hello, I am looking for help. I am using TMP123 and there are unexpected readings. The issue is the readings from the sensor are coming in mostly reasonable, but every few seconds will give a reading in the 200C-250C range. We are hoping…
Part Number: TMP123 Hello, TMP123 datasheet specified absolute maximum input voltage is 7V. Is this true regardless of V+ voltage? For example, if V+ = 3.3V, the maximum SCK input voltage could be 7V? Best regards, K.Hirano
Part Number: TMP121 Other Parts Discussed in Thread: TMP123 , TMP125 Hello,
Got a fairly straightforward question regarding the TMP121/TMP123 and was looking to see if someone could help clarify something regarding the SPI output.
What is the SPI SO pin…
Part Number: TMP123 Other Parts Discussed in Thread: LM70 , Hi , I am using TMP123AIDBVR temperature sensor and trying to interface it with the spi in our custom zynqmp board . 1. We need to know the device tree changes to register the temperature sensor…
Part Number: TMP123 Other Parts Discussed in Thread: TMP121 , Hello,
Can TMP121's IBIS model be used for TMP123? It seems the chips are similar and the only differences are pinjs 1&2 (which are gnd and NC) as well as temp range
Thank you!
Part Number: TMP123 Other Parts Discussed in Thread: TMP121 Let me ask about the relation between CS control and conversion time.
Datasheet of TMP123 describes the followings,
At "COMMUNICATING WITH THE TMP121" of APPLICATIONS INFROMATION in page5…
Part Number: TMP123 Let me question about the operation of TMP123.
[Malfunction] IQ (quiescent current) is specified as 50uA (max) in the data sheet. However, we actually consume about 15mA of current.
What is the cause of 15mA consumption?
[15mA consumption…
Part Number: TMP123 Other Parts Discussed in Thread: TMP125 Hi,
We are using TMP123 in our design. Somehow I missed to connect CS# pin to our microcontroller because of GPIO shortage and I directly pulled CS# pin to GND. Now when i am trying to read temperature…
Part Number: TMP123 Hi,
First effective data output timing after power supply
1)After VDD supply, is the first temperature conversion data valid data? or Will conversion data from the second time become effective after VDD supply?
2)After VDD supply…