Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TMP125 Hi,
Does anyone have a VHDL code to interface TMP125 with a CPLD. I wanted to check the working of the device in my prototype pls.
Thanks,
Arvind Gupta
Part Number: TMP125 Tool/software: Linux Hi I am trying to read data from the sensor. But all i am getting is a constant value 40206b00. This happens when I send a 0x3000 to put the device in one shot and shutdown mode and then read the latest converted…
Other Parts Discussed in Thread: TMP125 , CC2540 Hello,
I've some trouble understanding the one-shot mode of TMP125. Sorry if my question is stupid but first time doing this...
So as I understand it from the manual:
1) To enter shutdown mode:
nCS =…
Part Number: TMP121 Other Parts Discussed in Thread: TMP123 , TMP125 Hello,
Got a fairly straightforward question regarding the TMP121/TMP123 and was looking to see if someone could help clarify something regarding the SPI output.
What is the SPI SO pin…
Other Parts Discussed in Thread: TMP125 Hi
im a student .. for my project im using TMP125 temperature sensor connect to PIC24FJ256GB..
while reading temp register im not getting the actual temperature... From data sheet its saying it s a 16bit register…
Other Parts Discussed in Thread: TMP121 , TMP125 Hi,
I am looking for a simple SPI based temperature sensor to interface with a CPLD. Can anyone suggest the same. If possible, pls. suggest any DIP /SOT223 package which can be hand soldered.
Thanks and…
Part Number: TMP123 Other Parts Discussed in Thread: TMP125 Hi,
We are using TMP123 in our design. Somehow I missed to connect CS# pin to our microcontroller because of GPIO shortage and I directly pulled CS# pin to GND. Now when i am trying to read temperature…
Hello Daniel,
I've attached some sample code for the TMP125 and MSP430FG4618. While there are some differences between the TMP125 and TMP124, this code should provide a good starting point.
Best regards,
Ian Williams Linear Applications Engineer …
Other Parts Discussed in Thread: TMP112 , TMP121 , TMP125 , CC1101 Hello
I am planing to use tmp112 with pic mcu. spi is shared with i2c interface. i want to use hardware i2c so i need to wire them parallel. In pic i2c open draini so i need to use pull ups…
Hello Dan,
I've attached example code for the TMP125 to help get you started. Unfortunately this is the only example code for temp sensors that we have available. For further assistance, please post on the MSP430 support forum at: http://e2e.ti.com…