Part Number: TMP451-Q1 Other Parts Discussed in Thread: TMP127-Q1 , TMP126-Q1 , LM95071-Q1 , LM71-Q1 Hi, do you have such component but with SPI interface (not I2C)?
Ariel Greenbaum
Hello Tu,
The absolute maximum temperature rating for both operation and storage for TMP117 is 155°C, and the TMP117 should not be used beyond its abs max limit.
We dont have data to support using the TMP117 beyond its absolute maximum rating. If…
Part Number: TMP1075 Other Parts Discussed in Thread: TMP461 , LMT86 , TMP126 , Dear team,
We receive a question about how to calcualte the response time of the TI temp sensor. Such as TMP1075, TMP461, TMP126 and LMT86? From my understanding, the responsible…
Hi Ray Vincent,
We have several temperature sensors that can meet their accuracy and temperature range requirements, as shown in this parametric search [temperature range 50°C to 150°C, accuracy ±1°C (this can be adjusted depending on accuracy requirements…
Part Number: TMP116 Other Parts Discussed in Thread: TMP117 , , TMP126-Q1 , TMP126 Hello,
we are in search of an accurate temperature sensor (max. +/-0.3°C accuracy, like TMP116 or TMP117) for a test and measurement project.
The power consumption is…
Dear Yuki -
Thanks for the post - the EVM is made to have the TMP126 detached by breaking the board end off, at the header, to then connect to another MCU as you desire.
We have interfaced this part to other MSP430/SimpleLink LaunchPads and Ardunio/Energia…
Thanks a lot once again
1) In AFE4950EVM sensor board is included ??
2). For example, if I want to procure one of the following sensors mentioned and connect them to the Evaluation Modules you suggested (eg AFE4950EVM), should I procure the chip or hardware…