Part Number: TMP127-Q1 Other Parts Discussed in Thread: TMP127 , TMP1826 Tool/software: Hi,
Current FPGA only has two 3.3V unused IO. Can it interface with TMP127-Q1 via SIO and SCLK then leave CS stays low all the time?
Thanks,
Lawrence
Part Number: TMP127-Q1 Other Parts Discussed in Thread: TMP126 , TMP126-Q1 , TMP127 I have a previous post about issues with the tmp126: TMP126-Q1: Issues with multiple devices on SPI bus
In that post it was recommended to use the TMP127 instead, which…
Part Number: TMP127-Q1 Other Parts Discussed in Thread: TMP127 May I ask, if this temperature sensor uses a four-wire SPI communication system and needs to support a baud rate of 10M, what is the appropriate resistance value of this isolation resistor…
Part Number: TMP127-Q1 I am looking for I2C to SPI conversion device. The protocol converter device will be connected to a microcontroller as I2C slave. The microcontroller will send read/write commands to the I2C to SPI conversion device. Do we have…
Part Number: TMP127-Q1 Hi,
I have a free SPI line with 4 CS's and was thinking of using these instead of thermistors. Firstly am I right in thinking that i can put all 4 on the same SPI line and alternate CS for each? I do not need to put the devices…
Part Number: TMP126-Q1 Other Parts Discussed in Thread: TMP127-Q1 , , TMP127 , TMP126
Tool/software:
Dear team,
Can TMP126-Q1 work with Read-only mode? TMP127-Q1 supports according to the datasheet. We just want higher accuracy than TMP127 but #…
Part Number: TMP127-Q1 Other Parts Discussed in Thread: TMP127 Tool/software: I intend to use the TMP127-Q1 temperature sensor in 4- wire configuration:-
Now the specification for the rise time for the SIO line is 100ns max. This would seam difficult…
Part Number: TMP451-Q1 Other Parts Discussed in Thread: TMP127-Q1 , TMP126-Q1 , LM95071-Q1 , LM71-Q1 Hi, do you have such component but with SPI interface (not I2C)?
Ariel Greenbaum
Hi SunSet,
Thanks for posting to the Sensors forum.
The TMP126 and TMP127-Q1 do not have the same register structure.
The TMP126 register structure is noted in section 8.6 Register Map of the TMP126 datasheet. The Device ID for the TMP126 is 2126h…