Part Number: TMP1826-1-WIRE-CODE
Tool/software:
P/N TMP1826NGRR has about 100% failure rate. The sensors fare not providing any temperature reading, even though we can see the IP address.
Did you transmit Reset, SkipROM (0xCC), Read ScratchPad-1(0xBE) before the read byte loop?
From the datasheet:
See also GetTemperature() in tmp182x_func_driver.c included with TMP1826-1-WIRE-CODE download.
thanks,
ren
Part Number: TMP1826 Tool/software: Hi,
I'm dealing with a communication issue with the TMP1826 chip. I believe the timing is correct, as the chip reset, device detection, as well as data writing and reading are all working. This is supported by the…
Part Number: TM4C1294NCPDT Other Parts Discussed in Thread: TMP1826 I am looking for the code files associated with "Implementing 1-Wire Enumeration for TMP1826 With TM4C129x Microcontrollers", TI Lit#spma057. The link below, which was embedded in the…
Part Number: USB2ANY Tool/software:
Hi TI expert,
1) Does USB2ANY support th OneWire communication.
2) We have to validate the USB2ANY for OneWire communication. Does TI have any reference design or EVM kit with them that TI has tested for USB2ANY…
Part Number: MSPM0G3507 Other Parts Discussed in Thread: MSPM0G5117 Hi!
This is Ken, we currently use the MSPM0G5117 MCU on our product and we have MSPM3507 EVM. Due to connection interface has a limited number of pins, the MCU will communicate with…
Part Number: BQ79718B-Q1 Tool/software: Hi,
I tried clearing my questions since 7 days , but not getting any reply.
Trying again.
Is Afe Bq79718 having open wire detection Cell1-18 ?
Part Number: LP-MSPM0G3507 Other Parts Discussed in Thread: MSPM0G3507
Hi Team,
Posting on behalf of our customer.
I'm trying to use this example to doing fw update(MCU to MCU): \LP_MSPM0G3507\bsl\bsl_spi_flash_interface Change default SPI interface…
Part Number: LMH6553 Tool/software: LMH6553SD/NOPB all wire material is Gold are these Date code part 's wire material is Gold?
for example,
please see below Date code information:DC:2225+5 are these Date code part 's wire material is Gold?