Part Number: TMP236 Tool/software: I made a product that has a protection circuit that operates when overheated.
However, in order to verify, I have to force the voltage to increase on VOUT of TMP236. Is it okay to force DC1~3V to Vout using dc power…
Part Number: TMP236 Other Parts Discussed in Thread: TMP235 , ISOTMP35 Tool/software: Dear Friend
My application is to protect a linear Mosfet from overheating with possible heavy/overstressed usage. the Mosfet is surface mounted with its drain connected…
Part Number: TMP236-Q1
Dear Team, We are using TMP236AQDBZTQ1 in our ASIL-D compliance product. As the mentioned component is not ASIL qualified, I need to do component evaluation to use it in safety application. For the component evaluation, I require…
Part Number: TMP236 Hi Team,
Our customer will use multiple TMP236 analog temperature sensors a few centimeters away from the MCU thru cables and would like to know how to reinforced the circuit. I have checked some application notes but most of them…
Part Number: TMP236 Hello,
I was thinking of using this part to sense toroidal transformer temperature.
It would be mounted on the outside of the transformer directly over the windings on a small PCB.
Do you think the strong magnetic field in this…
Part Number: TMP236 Hi Sir,
We are using LTC2997HDCB now, could you help to recommend a pin to pin or similar function part to replace? Better to have stock/good supply.
Customer used L TC2997HDCB by placing it close to heat source (locally).
Thank…
Part Number: TMP236-Q1 I am working with TMP236-Q1 parts on a prototype board. According to the datasheet, the typical Tc is 19.5mV. However, measuring the mV output directly on 3 different sensors on temps ranging from 10C to 50C, the coefficient works…
Part Number: TMP236 I'm using SOT32 TMP236 analog temperature sensor. I mounted it with long pins far from the PCB to avoid heating from other components on the board. So the sensor is now "floating" in the air.
The output voltage is around 1.0V (35…
Igor -
TMP23x family has two gain options, as indicated first on the front page of the data sheet. If you require the wider temp range support, you can replace TMP236 directly with TMP235. With regards to the wording of the datasheet, consider operating…
Part Number: TMP235 Other Parts Discussed in Thread: TMP236 My customer HEMAI is using out TMP235 and syslink's CT7035 for P2P. And they are cusrious about the sensor gain parameter in the datasheet .
So what performance the sensor gain of a temperature…