Part Number: TMP275-Q1 Other Parts Discussed in Thread: TMP275
Is it possible for the device to be in shut-down mode initially and then triggered to do a One-Shot conversion? What are the ramifications of triggering a one-shot conversion by setting the…
Part Number: TMP275 Other Parts Discussed in Thread: TPS82130 We have a few TMP275 sensors spread around in a system, connected by wires, and powered by a 5v TPS82130 (powering also some other relatively light loads).
What should be the 5v PS specifications…
Part Number: TMP275 Other Parts Discussed in Thread: TMP114 I am planning on using the TMP275 for on board temp sensing. It runs off 3.3V, but looking at the digital logic threshold, it's not possible to interface with 1.5V LVCMOS logic. Is there a solution…
Part Number: TMP275 Hi Team,
I aksed TMP275 I2C quetion in below e2e but I have additional question so could you hlep?
[Question 1] TMP275 reqires conversion time for conversion result. if we READ before finishing conversion time, what is the output data…
Part Number: TMP275 What are the ramifications of using a 1 kOhm pull up on a 5V line driving the TMP275AIDR? The data sheet states 3 mA maximum, but the design is working with the 1 kOhm pullup (5mA) in the lab. The I2C bus has 8 different devices on…
Part Number: TMP275 I need a temperature sensor recommendation with the following key specification:
3.3V Powered
I2C Interface with at least four addresses
-10 to 85°C range (min)
Isolated from ground sensing.
The last requirement is important and…
Hi Jimmy,
We offer many different device packages because of different # of pins, PCB area concerns, and other customer needs. Whichever sensor you choose, it is still important to follow ensure low thermal conductivity between the PCB and the temperature…
Part Number: TMP275 Hi Team, Is the TMP275 sensitive to X-Ray? Asking this as our customer is using X-ray for their component count and PCBA inspection. In case the device is x-ray sensitive, what are the critical parameters/factors to the device that we…
Part Number: TMP275 Other Parts Discussed in Thread: TMP1075 Please tell me.
Is it correct to understand that the temperature is updated every Conversion Time when used in Comparator Mode?
Does changing the Converter Resolution change the frequency of…