Part Number: TMP302 Other Parts Discussed in Thread: TMP303 Hi Professional,
My customer look for Temp sensor which has ratch type ouput. And the other specification is similar as TMP302.
Do you have any appropriate product for this requirement?
Best…
Part Number: TMP302 THS Support team
How much is the minimum value of supply voltage of the absolute maximum rating? I think that it should be added to the datasheet.
Thanks
Tamio
Part Number: TMP302 Hi, Team!
I need to install sensor TMP302 to D-pack diode width D-pack cooler.
How to install sensor TMP302 correctly? I use SMD mount and sensor TMP302 in
micropackage SOT563. How to provide termo connection? Maybe you have photo?
Best…
Part Number: TMP302 Other Parts Discussed in Thread: TMP303 , LM26NV Could you recommend products for OUT pin remains high when the temperature is at or above the selected temperature threshold.
Part Number: TMP302 Hi
Below is my questions about TMP302.
1. TMP302 maximum output current is 10mA, in which conditions?
2. I want to drive TMP302 with VRTC, VRTC maximum output capacity is 2mA, when system is shutdown, consume 0.1mA, can 1.9mA meet TMP302…
Part Number: TMP303 Other Parts Discussed in Thread: TMP302 , Hello all,
for a safety relevant development I have to be sure there is no software-part at all components. I'm planning to use TMP302 or TMP303 for temperature-shutdown.
I think, these chips…
Part Number: TMP302 Hi,
Can you confirm that
TMP302 output cannot be low during first 35ms after power-up when T < Ttrip? (as shown in datasheet figure 12)
TMP302 output cannot be low during power down or when Vs temporarily drops below 1.4V (eg…
Part Number: TMP302 I want to measure the temperature of a voltage plane. This voltage plane is my heat source as indicated in Figure 14 of TMP302 datasheet. Figure 14 indicates a "Ground Plane for Thermal Coupling to Heat Source". Is this a signal Ground…