Part Number: TMP302-Q1 Hello Experts, My customer would like to know where the temp sensor is located in the chip. Would you tell it, please? Best Regards, Fujiwara
Part Number: TMP302-Q1 Hello,
According to TMP302-Q1 datasheet, if HYSTSET pin connect to GND, THRESHOLD HYSTERESIS is 5°C, if connect to Vs, it's 10°C.
What is THRESHOLD HYSTERESIS if HYSTSET pin left floating?
What kind of symptom is occurred…
Part Number: TMP302-Q1 Other Parts Discussed in Thread: TMP302 Hi there
We are looking at using the TMP302C in an application providing thermal (over temperature) safety protection - its very attractive for this due to its precise temperature accuracy…
Hi Keith,
The DFMEA of TMP302-Q1 is available through a PPAP request. However, this document is not the same as a functional safety FMEA (if that is what you are referring to) as it does not include FITs or failure mode distributions.
Best regards…
Dear Art -
This device that you pointed to is a physical single pole thermal (bi-metallic) switch which is used directly inline with distributed and higher system voltages. From our product line of silicon based products, for you to provide a drop in…
Other Parts Discussed in Thread: LM5069 , LM5069EVM-627 , CSD19536KTT , TMP302 , LM5066I Hello,
I have a question regarding the input voltage clamping of the LM5069.
We have implemented a circuit similar the the EVM: LM5069EVM-627. Now i have…
Part Number: TIDA-00701 Other Parts Discussed in Thread: UCC28051
Hi,
I am designing a 100W 24V power supply as detailed in design note tida-00701 and I have a few queries regarding the design:-
1) Page number 45 section 7.4 of the design note says…